public static class EndCutBuilder.ConnectionTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CONNECTED
If this Connection Type is set, the offset parameter will be ignored.
|
static int |
_FLANGE_FREE
If this Connection Type is set, the offset parameter will be ignored.
|
static int |
_SNIPED
If this Connection Type is set, the offset parameter can be used.
|
static EndCutBuilder.ConnectionTypes |
CONNECTED
If this Connection Type is set, the offset parameter will be ignored.
|
static EndCutBuilder.ConnectionTypes |
FLANGE_FREE
If this Connection Type is set, the offset parameter will be ignored.
|
static EndCutBuilder.ConnectionTypes |
SNIPED
If this Connection Type is set, the offset parameter can be used.
|
Modifier and Type | Method and Description |
---|---|
static EndCutBuilder.ConnectionTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EndCutBuilder.ConnectionTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EndCutBuilder.ConnectionTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final EndCutBuilder.ConnectionTypes CONNECTED
public static final EndCutBuilder.ConnectionTypes FLANGE_FREE
public static final EndCutBuilder.ConnectionTypes SNIPED
public static final int _CONNECTED
public static final int _FLANGE_FREE
public static final int _SNIPED
public static EndCutBuilder.ConnectionTypes valueOf(int value)
public static EndCutBuilder.ConnectionTypes valueOf(String name)
public static EndCutBuilder.ConnectionTypes[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.