public static class ShellTemplateBuilder.PlaneLocationTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_EXISTING
Use existing planes to define the individual template locations.
|
static int |
_OFFSET
Derive the plane locations from the orientation coordinate system or X and Y specified base planes
|
static ShellTemplateBuilder.PlaneLocationTypes |
EXISTING
Use existing planes to define the individual template locations.
|
static ShellTemplateBuilder.PlaneLocationTypes |
OFFSET
Derive the plane locations from the orientation coordinate system or X and Y specified base planes
|
Modifier and Type | Method and Description |
---|---|
static ShellTemplateBuilder.PlaneLocationTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ShellTemplateBuilder.PlaneLocationTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ShellTemplateBuilder.PlaneLocationTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final ShellTemplateBuilder.PlaneLocationTypes EXISTING
public static final ShellTemplateBuilder.PlaneLocationTypes OFFSET
public static final int _EXISTING
public static final int _OFFSET
public static ShellTemplateBuilder.PlaneLocationTypes valueOf(int value)
public static ShellTemplateBuilder.PlaneLocationTypes valueOf(String name)
public static ShellTemplateBuilder.PlaneLocationTypes[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.