public static class PillarBuilder.CreationMethod extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ADOPTION |
static int |
_POINTS |
static int |
_SPECIFY_CSYS |
static int |
_SPECIFY_LINE |
static int |
_STRUCTURE |
static int |
_TWO_PLANESAND_LINES |
static PillarBuilder.CreationMethod |
ADOPTION |
static PillarBuilder.CreationMethod |
POINTS |
static PillarBuilder.CreationMethod |
SPECIFY_CSYS |
static PillarBuilder.CreationMethod |
SPECIFY_LINE |
static PillarBuilder.CreationMethod |
STRUCTURE |
static PillarBuilder.CreationMethod |
TWO_PLANESAND_LINES |
Modifier and Type | Method and Description |
---|---|
static PillarBuilder.CreationMethod |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PillarBuilder.CreationMethod |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PillarBuilder.CreationMethod[] |
values()
Returns an array that contains the values for this enum.
|
public static final PillarBuilder.CreationMethod TWO_PLANESAND_LINES
public static final PillarBuilder.CreationMethod SPECIFY_LINE
public static final PillarBuilder.CreationMethod SPECIFY_CSYS
public static final PillarBuilder.CreationMethod ADOPTION
public static final PillarBuilder.CreationMethod STRUCTURE
public static final PillarBuilder.CreationMethod POINTS
public static final int _TWO_PLANESAND_LINES
public static final int _SPECIFY_LINE
public static final int _SPECIFY_CSYS
public static final int _ADOPTION
public static final int _STRUCTURE
public static final int _POINTS
public static PillarBuilder.CreationMethod valueOf(int value)
public static PillarBuilder.CreationMethod valueOf(String name)
public static PillarBuilder.CreationMethod[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.