public static class ShipEndCutBuilder.CreationMethod extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FACE_EDGE
1 face and 1 edge are used to place this endcut
|
static int |
_SPECIFY_CSYS
a csys is used to place this endcut
|
static ShipEndCutBuilder.CreationMethod |
FACE_EDGE
1 face and 1 edge are used to place this endcut
|
static ShipEndCutBuilder.CreationMethod |
SPECIFY_CSYS
a csys is used to place this endcut
|
Modifier and Type | Method and Description |
---|---|
static ShipEndCutBuilder.CreationMethod |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ShipEndCutBuilder.CreationMethod |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ShipEndCutBuilder.CreationMethod[] |
values()
Returns an array that contains the values for this enum.
|
public static final ShipEndCutBuilder.CreationMethod FACE_EDGE
public static final ShipEndCutBuilder.CreationMethod SPECIFY_CSYS
public static final int _FACE_EDGE
public static final int _SPECIFY_CSYS
public static ShipEndCutBuilder.CreationMethod valueOf(int value)
public static ShipEndCutBuilder.CreationMethod valueOf(String name)
public static ShipEndCutBuilder.CreationMethod[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.