public static class PlateStockBuilder.ThickenOptions extends Enum
PlateStockBuilder
.Modifier and Type | Field and Description |
---|---|
static int |
_SINGLE_SIDED
Thickness is applied to only the front side of the offset mold face.
|
static int |
_SYMMETRIC
Half of the thickness is applied to back and front sides of the offset mold face.
|
static int |
_TWO_SIDED
The opposite thickness is applied to the back side of the offset mold face, thickness minus the opposite thickness is applied to the front side of the offset mold face.
|
static PlateStockBuilder.ThickenOptions |
SINGLE_SIDED
Thickness is applied to only the front side of the offset mold face.
|
static PlateStockBuilder.ThickenOptions |
SYMMETRIC
Half of the thickness is applied to back and front sides of the offset mold face.
|
static PlateStockBuilder.ThickenOptions |
TWO_SIDED
The opposite thickness is applied to the back side of the offset mold face, thickness minus the opposite thickness is applied to the front side of the offset mold face.
|
Modifier and Type | Method and Description |
---|---|
static PlateStockBuilder.ThickenOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PlateStockBuilder.ThickenOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PlateStockBuilder.ThickenOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final PlateStockBuilder.ThickenOptions SINGLE_SIDED
public static final PlateStockBuilder.ThickenOptions TWO_SIDED
public static final PlateStockBuilder.ThickenOptions SYMMETRIC
public static final int _SINGLE_SIDED
public static final int _TWO_SIDED
public static final int _SYMMETRIC
public static PlateStockBuilder.ThickenOptions valueOf(int value)
public static PlateStockBuilder.ThickenOptions valueOf(String name)
public static PlateStockBuilder.ThickenOptions[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.