public static class OrientationAngleMethodsBuilder.MethodTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ALIGNED
Angle is the same as the previous or following region.
|
static int |
_ANGLE
Angle is defined by specifying a constant angle from a reference object.
|
static int |
_VECTOR
Angle is defined by specifying a vector to align with.
|
static OrientationAngleMethodsBuilder.MethodTypes |
ALIGNED
Angle is the same as the previous or following region.
|
static OrientationAngleMethodsBuilder.MethodTypes |
ANGLE
Angle is defined by specifying a constant angle from a reference object.
|
static OrientationAngleMethodsBuilder.MethodTypes |
VECTOR
Angle is defined by specifying a vector to align with.
|
Modifier and Type | Method and Description |
---|---|
static OrientationAngleMethodsBuilder.MethodTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OrientationAngleMethodsBuilder.MethodTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OrientationAngleMethodsBuilder.MethodTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final OrientationAngleMethodsBuilder.MethodTypes ANGLE
public static final OrientationAngleMethodsBuilder.MethodTypes VECTOR
public static final OrientationAngleMethodsBuilder.MethodTypes ALIGNED
public static final int _ANGLE
public static final int _VECTOR
public static final int _ALIGNED
public static OrientationAngleMethodsBuilder.MethodTypes valueOf(int value)
public static OrientationAngleMethodsBuilder.MethodTypes valueOf(String name)
public static OrientationAngleMethodsBuilder.MethodTypes[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.