public static class EdgeCutBuilder.ArraySpacing extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CUSTOM_DEFINED
The user can specify a custom amount of space between the cuts
|
static int |
_EVEN_DISTRIBUTION
Cuts will automatically be spaced evenly along the length of the guide
|
static EdgeCutBuilder.ArraySpacing |
CUSTOM_DEFINED
The user can specify a custom amount of space between the cuts
|
static EdgeCutBuilder.ArraySpacing |
EVEN_DISTRIBUTION
Cuts will automatically be spaced evenly along the length of the guide
|
Modifier and Type | Method and Description |
---|---|
static EdgeCutBuilder.ArraySpacing |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EdgeCutBuilder.ArraySpacing |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EdgeCutBuilder.ArraySpacing[] |
values()
Returns an array that contains the values for this enum.
|
public static final EdgeCutBuilder.ArraySpacing EVEN_DISTRIBUTION
public static final EdgeCutBuilder.ArraySpacing CUSTOM_DEFINED
public static final int _EVEN_DISTRIBUTION
public static final int _CUSTOM_DEFINED
public static EdgeCutBuilder.ArraySpacing valueOf(int value)
public static EdgeCutBuilder.ArraySpacing valueOf(String name)
public static EdgeCutBuilder.ArraySpacing[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.