Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static EdgeCutBuilder.ArraySpacing |
EdgeCutBuilder.ArraySpacing.CUSTOM_DEFINED
The user can specify a custom amount of space between the cuts
|
static EdgeCutBuilder.ArraySpacing |
EdgeCutBuilder.ArraySpacing.EVEN_DISTRIBUTION
Cuts will automatically be spaced evenly along the length of the guide
|
Modifier and Type | Method and Description |
---|---|
EdgeCutBuilder.ArraySpacing |
EdgeCutBuilder.spacing()
Returns the spacing (even distribution or custom defined)
License requirements: None. |
static EdgeCutBuilder.ArraySpacing |
EdgeCutBuilder.ArraySpacing.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EdgeCutBuilder.ArraySpacing |
EdgeCutBuilder.ArraySpacing.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EdgeCutBuilder.ArraySpacing[] |
EdgeCutBuilder.ArraySpacing.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EdgeCutBuilder.setSpacing(EdgeCutBuilder.ArraySpacing spacing)
License requirements: nx_ship_detail ("Ship Detail Design") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.