public static class LongitudinalBulkheadBuilder.Types extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_EXTRUSION
Mold face is being defined by extruding a supplied section shape.
|
static int |
_PLANES
Mold face is being defined by selected or defined planes.
|
static int |
_SHEET_BODY
Mold face is being defined by a selected sheet body.
|
static LongitudinalBulkheadBuilder.Types |
EXTRUSION
Mold face is being defined by extruding a supplied section shape.
|
static LongitudinalBulkheadBuilder.Types |
PLANES
Mold face is being defined by selected or defined planes.
|
static LongitudinalBulkheadBuilder.Types |
SHEET_BODY
Mold face is being defined by a selected sheet body.
|
Modifier and Type | Method and Description |
---|---|
static LongitudinalBulkheadBuilder.Types |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LongitudinalBulkheadBuilder.Types |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LongitudinalBulkheadBuilder.Types[] |
values()
Returns an array that contains the values for this enum.
|
public static final LongitudinalBulkheadBuilder.Types SHEET_BODY
public static final LongitudinalBulkheadBuilder.Types PLANES
public static final LongitudinalBulkheadBuilder.Types EXTRUSION
public static final int _SHEET_BODY
public static final int _PLANES
public static final int _EXTRUSION
public static LongitudinalBulkheadBuilder.Types valueOf(int value)
public static LongitudinalBulkheadBuilder.Types valueOf(String name)
public static LongitudinalBulkheadBuilder.Types[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.