public static class PenetrationRequest.RequestType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_MULTIPLE |
static int |
_SINGLE |
static PenetrationRequest.RequestType |
MULTIPLE |
static PenetrationRequest.RequestType |
SINGLE |
Modifier and Type | Method and Description |
---|---|
static PenetrationRequest.RequestType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PenetrationRequest.RequestType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PenetrationRequest.RequestType[] |
values()
Returns an array that contains the values for this enum.
|
public static final PenetrationRequest.RequestType SINGLE
public static final PenetrationRequest.RequestType MULTIPLE
public static final int _SINGLE
public static final int _MULTIPLE
public static PenetrationRequest.RequestType valueOf(int value)
public static PenetrationRequest.RequestType valueOf(String name)
public static PenetrationRequest.RequestType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.