public interface HullBuilder extends PlateSystemBuilder
Hull
feature.
ShipCollection.createHullBuilder(nxopen.features.shipdesign.Hull)
Property | Value |
---|---|
Offset.Value | 0 (millimeters part), 0 (inches part) |
Primary | FwdPortToInUp |
PrimaryOnReference | FwdPortToInUp |
Secondary1 | FwdPortToInUp |
Secondary1OnReference | FwdPortToInUp |
Secondary2 | FwdPortToInUp |
Secondary2OnReference | FwdPortToInUp |
Modifier and Type | Interface and Description |
---|---|
static class |
HullBuilder.Types
Indicates the method that is being used to define the mold face of the hull.
|
PlateSystemBuilder.StiffenerDirectionType
FeatureParmsBuilder.OrientationAngleRuleTypes
Modifier and Type | Method and Description |
---|---|
ScCollector |
moldFaces()
Returns the faces selected that defines the overall shape of the hull.
|
SelectBody |
moldFaceSheet()
Returns the sheet body selected that defines the overall shape of the hull.
|
void |
setType(HullBuilder.Types type)
License requirements: nx_ship_basic ("Ship Basic Design") . |
HullBuilder.Types |
type()
Returns the method used to define the mold face of the hull.
|
boundaryPlane, boundarySection, boundarySheets, cleanUpTemporaryCurves, createRegionBody, deletePreviewBody, deleteRegionBody, offset, primary, primaryOnReference, projectionDirection, regions, secondary1, secondary1OnReference, secondary2, secondary2OnReference, setBoundaryPlane, setKnuckleEdges, setPreviewOption, setPrimary, setPrimaryOnReference, setRegionIndex, setRegionPoints, setSecondary1, setSecondary1OnReference, setSecondary2, setSecondary2OnReference, setSplitEdgeUpdateFlag, setTightness, shipNames, splitKnuckleEdges, stock, thicknessDirection, tightness, weld
angleTolerance, createPlaneForList, distanceTolerance, orientationAngleRule, setAngleTolerance, setDistanceTolerance, setOrientationAngleRule
SelectBody moldFaceSheet() throws NXException, RemoteException
HullBuilder.Types.SHEET_BODY
is set.
NXException
RemoteException
ScCollector moldFaces() throws NXException, RemoteException
HullBuilder.Types.FACES
is set.
NXException
RemoteException
HullBuilder.Types type() throws NXException, RemoteException
NXException
RemoteException
void setType(HullBuilder.Types type) throws NXException, RemoteException
type
- NXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.