public static class EndCutBuilder.DraftTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_EXTEND
If this Draft Type is set, the EndCut face will split and the right side face will be tapered.
|
static int |
_TRIM
If this Draft Type is set, the EndCut face will split and the left side face will be tapered.
|
static EndCutBuilder.DraftTypes |
EXTEND
If this Draft Type is set, the EndCut face will split and the right side face will be tapered.
|
static EndCutBuilder.DraftTypes |
TRIM
If this Draft Type is set, the EndCut face will split and the left side face will be tapered.
|
Modifier and Type | Method and Description |
---|---|
static EndCutBuilder.DraftTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EndCutBuilder.DraftTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EndCutBuilder.DraftTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final EndCutBuilder.DraftTypes TRIM
public static final EndCutBuilder.DraftTypes EXTEND
public static final int _TRIM
public static final int _EXTEND
public static EndCutBuilder.DraftTypes valueOf(int value)
public static EndCutBuilder.DraftTypes valueOf(String name)
public static EndCutBuilder.DraftTypes[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.