NXOpen.Weld Package¶
Classes¶
NXOpen.Weld.AutoPoint |
This class will automatically create weld points from selected components |
NXOpen.Weld.AutoPointBuilder |
Represents a NXOpen.Weld.AutoPointBuilder builder |
NXOpen.Weld.AutoWeldSymbolsBuilder |
Represents a NXOpen.Weld.AutoWeldSymbolsBuilder builder |
NXOpen.Weld.CharacteristicsBuilder |
This builder allows you to define the attribute values to be set on the output of the weld feature. |
NXOpen.Weld.CharacteristicsSelectionBuilder |
This builder allows you to define the attribute values to be set on the output of the weld feature. |
NXOpen.Weld.CharacteristicsValueBuilder |
The object containing the information about the attribute to be placed on the output of the weld feature. |
NXOpen.Weld.CompoundWeld |
Represents a compound weld feature. |
NXOpen.Weld.CompoundWeldBuilder |
Represents a NXOpen.Weld.CompoundWeld builder. |
NXOpen.Weld.ConnectedFaceFinderBuilder |
Represents a builder to run the Connected Face Finder operation. |
NXOpen.Weld.ConnectionFinderBuilder |
Represents a builder to display, manage, delete, and allow the user to reparent face information for the weld objects. |
NXOpen.Weld.CustomManager |
Represents weld interface to customize the creation of welding joint features. |
NXOpen.Weld.DatumCommonBuilder |
Used to create or edit a NXOpen.Weld.DatumSurface or NXOpen.Weld.DatumPin feature. |
NXOpen.Weld.DatumIconBuilder |
Represents a NXOpen.Weld.DatumIconBuilder class used to control the part navigator icon for Datum Pin and Surface Locators. |
NXOpen.Weld.DatumPin |
Represents a Weld Datum Pin feature |
NXOpen.Weld.DatumPinBuilder |
Used to create or edit a NXOpen.Weld.DatumPin feature. |
NXOpen.Weld.DatumSurface |
Represents a Weld Datum Surface feature |
NXOpen.Weld.DatumSurfaceBuilder |
Used to create or edit a NXOpen.Weld.DatumSurface feature. |
NXOpen.Weld.EasyPatternBuilder |
Represents the easy pattern builder. |
NXOpen.Weld.EdgePrep |
Represents a Weld Edge Prep feature |
NXOpen.Weld.EdgePrepBuilder |
A builder used to create or edit a NXOpen.Weld.EdgePrep feature. |
NXOpen.Weld.EdgePrepValuesBuilder |
Used to view or edit the values used to define the welding joint and edge preparation. |
NXOpen.Weld.ExportWeldBuilder |
Represents a ExportWeldBuilder class |
NXOpen.Weld.ExportWeldJointBuilder |
Represents exporting weld joints. |
NXOpen.Weld.Extract |
Represents a Linked Feature created in the Weld Assistant. |
NXOpen.Weld.Fill |
Represents a Weld Fill feature |
NXOpen.Weld.Fillet |
Represents a Weld Fillet Feature. |
NXOpen.Weld.FilletBuilder |
Represents a NXOpen.Weld.Fillet builder. |
NXOpen.Weld.Groove |
Represents a WeldGroove feature. |
NXOpen.Weld.GrooveBuilder |
Represents a Groove Weld feature |
NXOpen.Weld.InformationBuilder |
This class is used by “Fabrication Information” to output fabrication objects information. |
NXOpen.Weld.JointExitBuilder |
Used to set custom edge preparation parameters of a NXOpen.Weld.WeldJoint feaure. |
NXOpen.Weld.JointItemBuilder |
Used to create or edit a Weld.WeldJoint feature. |
NXOpen.Weld.JointItemBuilderList |
Represents a list of objects. |
NXOpen.Weld.Jointmark |
Represents a Weld Jointmark Feature. |
NXOpen.Weld.JointmarkBuilder |
Represents a NXOpen.Weld.Jointmark builder |
NXOpen.Weld.JointmarkFaceSetsBuilder |
Used to create or edit a set of faces for Jointmark |
NXOpen.Weld.JointmarkFaceSetsBuilderList |
Represents a list of objects. |
NXOpen.Weld.JointmarkGuideBuilder |
Used to create or edit a guide curve for Jointmark. |
NXOpen.Weld.JointmarkGuideBuilderList |
Represents a list of objects. |
NXOpen.Weld.JointmarkPointsBuilder |
Used to create or edit a point in the list of points for Jointmark |
NXOpen.Weld.JointmarkPointsBuilderList |
Represents a list of objects. |
NXOpen.Weld.PlugSlot |
create a PlugSlot feature for Weld |
NXOpen.Weld.PlugSlotBuilder |
Represents a NXOpen.Weld.PlugSlot builder |
NXOpen.Weld.PointMark |
Represents a Weld PointMark Feature. |
NXOpen.Weld.PointMarkBuilder |
Used to create or edit a NXOpen.Weld.PointMark feature. |
NXOpen.Weld.PointMarkPoint |
Represents a Weld. |
NXOpen.Weld.PointMarkPointBuilder |
Used to create or edit a point in the list of points for Jointmark |
NXOpen.Weld.SelectDatumPin |
Represents a single object selection. |
NXOpen.Weld.SelectDatumSurface |
Represents a single object selection. |
NXOpen.Weld.StructureWeldBuilder |
This class is used to create or edit the information shared among all Structure Weld builders. |
NXOpen.Weld.SurfaceWeld |
Represents a surface weld feature |
NXOpen.Weld.SurfaceWeldBuilder |
Use to create or edit a NXOpen.Weld.SurfaceWeld feature. |
NXOpen.Weld.UserDefinedWeld |
Represents a User Defined Weld feature. |
NXOpen.Weld.UserDefinedWeldBuilder |
Represents a NXOpen.Weld.UserDefinedWeldBuilder builder. |
NXOpen.Weld.WeldAdvisorBuilder |
Represents a weld advisor test |
NXOpen.Weld.WeldBead |
Represents a Weld Bead feature |
NXOpen.Weld.WeldBeadBuilder |
Used to create or edit a NXOpen.Weld.WeldBead feature. |
NXOpen.Weld.WeldBeadPathBuilder |
Represents the path the bead shape will be swept along. |
NXOpen.Weld.WeldBeadPathBuilderList |
Represents a list of objects. |
NXOpen.Weld.WeldBeadSizeBuilder |
This builder is used to define the bead shape. |
NXOpen.Weld.WeldBeadSizeBuilderList |
Represents a list of objects. |
NXOpen.Weld.WeldCpdUtils |
Provides methods for access a WeldCpdUtils class object in NX. |
NXOpen.Weld.WeldFillBuilder |
A builder used to create or edit a NXOpen.Weld.Fill feature. |
NXOpen.Weld.WeldFillStripBuilder |
A builder used to create or edit a single strip of the NXOpen.Weld.WeldFillBuilder . |
NXOpen.Weld.WeldFillStripBuilderList |
Represents a list of objects. |
NXOpen.Weld.WeldGroove |
Represents a Weld Groove Feature |
NXOpen.Weld.WeldGrooveBuilder |
Represents a NXOpen.Weld.WeldGroove builder |
NXOpen.Weld.WeldImportBuilder |
Creates Weld features by reading a csv file |
NXOpen.Weld.WeldJoint |
Represents a weld joint feature |
NXOpen.Weld.WeldJointBuilder |
Used to create or edit a NXOpen.Weld.WeldJoint feature. |
NXOpen.Weld.WeldLabelBuilder |
Create weld labels for multiple welds and BIW locators, this builder’s Commit can produce more than one object, the GetCommittedObjects can be used to get the objects and the order of GetCommittedObject’s output array is stable. |
NXOpen.Weld.WeldManager |
Manages weld features and assistant tools. |
NXOpen.Weld.WeldObjectBuilder |
Represents a NXOpen.Weld.WeldObjectBuilder class used to collect welding objects created or edited from a command. |
NXOpen.Weld.WeldPmiBuilder |
Create PMI symbols for multiple structure welds, this builder’s Commit can produce more than one object, the GetCommittedObjects can be used to get the objects and the order of GetCommittedObject’s output array is stable. |
NXOpen.Weld.WeldPoint |
Represents a WeldPoint feature. |
NXOpen.Weld.WeldPointBuilder |
Represents a Spot Weld feature |
NXOpen.Weld.WeldPointExitBuilder |
Represents a NXOpen.Weld.WeldPointExitBuilder class used to pass welding object from the Weld Point command to a user callback. |
NXOpen.Weld.WeldPreferenceBuilder |
Represents a NXOpen.Weld.WeldPreferenceBuilder builder |
Enumerations¶
AutoPointBuilderInterferenceDetails Enumeration | Settings to indicate whether an interference is near an existing weld point. |
AutoPointBuilderTypes Enumeration | Settings to indicate whether new features should be created, or if features will be reused. |
CharacteristicsBuilderType Enumeration | The custom type of the datum specified for creation. |
CharacteristicsValueBuilderType Enumeration | Settings to indicate the type of value contained in the attribute. |
ConnectionFinderBuilderFilterTypes Enumeration | Filter values to control Save All processing. |
DatumCommonBuilderControlMethodTypes Enumeration | Settings for the method used to define the control direction. |
DatumCommonBuilderCreationDirectionMethods Enumeration | Settings to define the creation direction. |
DatumCommonBuilderCustomTypes Enumeration | The custom type of the datum specified for creation. |
DatumCommonBuilderSolidTypes Enumeration | Settings for defining the solid type to create for the datum object. |
DatumSurfaceBuilderTypes Enumeration | Settings to indicate the construction type used for the datum surface. |
EasyPatternBuilderHemMethodTypes Enumeration | Indicates the method to use to compute the hem vector location. |
EasyPatternBuilderPlaneMethodTypes Enumeration | The plane to cut sections in to determine placement measurement patterns. |
EasyPatternBuilderSpacingMethodTypes Enumeration | Indicates whether planes should be cut a grid lines, or if a single plane should be used. |
EasyPatternBuilderTypes Enumeration | Controls the type of pattern. |
EdgePrepValuesBuilderApply Enumeration | Option to indicate how the values are to be updated. |
EdgePrepValuesBuilderOption Enumeration | Option to indicate how the values are to be used. |
ExportWeldBuilderAttributeOriginType Enumeration | the Attribute Origin enum |
ExportWeldBuilderOutputType Enumeration | the Output Type enum |
FilletBuilderEnumConstructionMethod Enumeration | the options for which construction method to use. |
FilletBuilderEnumContour Enumeration | the Contour enum. |
FilletBuilderEnumExtendEdges Enumeration | the options for populating the edge selections. |
FilletBuilderEnumExtensionMethod Enumeration | the Extension enum. |
FilletBuilderEnumSkipWeldMethod Enumeration | the Skipweld enum. |
FilletBuilderEnumWeldingType Enumeration | the WeldingType enum. |
InformationBuilderAttributeOriginType Enumeration | the Object Type enum |
JointExitBuilderBodySide Enumeration | Settings to indicate the side the positions should be applied to. |
JointExitBuilderPositions Enumeration | Settings to indicate the desired position of edge preporation thickness and angle. |
JointmarkBuilderConnectedPanelTypes Enumeration | The type of sheets to create |
JointmarkBuilderMethod Enumeration | The type of construction method for creating Jointmark |
JointmarkBuilderOrientationMethodTypes Enumeration | The type of orientation method for defining the default coordinate system. |
JointmarkBuilderReferenceSheetTypes Enumeration | The type of sheets to create |
JointmarkGuideBuilderLocation Enumeration | The type of guide curve |
JointmarkGuideBuilderSpaceMethod Enumeration | Options for Spacing Method |
JointmarkGuideBuilderSpaceOption Enumeration | Spacing Option |
JointmarkPointsBuilderPointPosition Enumeration | The point classification |
OutputType Enumeration | Settings for output type |
PlugSlotBuilderArcProcessEnum Enumeration | arc process for the weld feature |
PlugSlotBuilderEnumContour Enumeration | contour type |
PointMarkBuilderWeldTypes Enumeration | The weld type to create. |
SurfaceWeldBuilderDestinationTypes Enumeration | The option specifying where the surface weld feature should be created. |
WeldAdvisorCheckerType Enumeration | the type of checker |
WeldAdvisorCustomerDefault Enumeration | the customer default value types |
WeldArcMethod Enumeration | Settings for output type |
WeldAttribType Enumeration | the type of attribute |
WeldBeadBuilderBeadLocationMethod Enumeration | Settings to indicate the desired location of the bead. |
WeldBeadBuilderOutputTypes Enumeration | Settings to indicate the update behaviour of the bead feature |
WeldBeadBuilderTypes Enumeration | Settings to indicate the sweep shape of the bead. |
WeldBeadPathBuilderOffsetMethodType Enumeration | Settings to indicate the desired offset method. |
WeldBeadSizeBuilderSize Enumeration | Settings to indicate which standard size to use from the customer defaults file. |
WeldContourShape Enumeration | Top contour shape |
WeldCreationDirection Enumeration | the type of creation direction |
WeldCustom Enumeration | Settings for output solid type |
WeldDatumControlDirection Enumeration | the control direction for datum |
WeldFacesetIndex Enumeration | the index of user picked face sets |
WeldFeatureOutput Enumeration | Feature output |
WeldFeatureSetType Enumeration | the feature set types |
WeldFillBuilderBoundaryMethodType Enumeration | Defines whether the initial boundary of the fill pattern is defined by a two point rectangle or a curve. |
WeldFillBuilderWidthAlongType Enumeration | Defines the direction the fill strip’s length is aligned |
WeldGrooveBuilderContour Enumeration | The options for Contour Type |
WeldGrooveBuilderEdge Enumeration | A value indicating whether the edges have been prepared |
WeldGrooveBuilderPrepare Enumeration | The type of edges to be prepared |
WeldGrooveBuilderSkipWeldMethod Enumeration | The options for creating Skip Weld |
WeldGrooveBuilderTaper Enumeration | The type of Taper Method |
WeldGrooveBuilderTypes Enumeration | The types of Groove to create |
WeldGrooveExtension Enumeration | Groove Extension Type |
WeldGrooveShape Enumeration | Groove Weld Section type |
WeldGrooveType Enumeration | Groove Creation Type |
WeldGroupIdColor Enumeration | the group id color indexes |
WeldJointBuilderApplication Enumeration | Application where joints are created. |
WeldJointBuilderCoordinateSystem Enumeration | Coordinate system specification. |
WeldJointBuilderDestinationTypes Enumeration | Where to create new joints. |
WeldJointBuilderSplitTypes Enumeration | Joint splitting options. |
WeldJointBuilderTypes Enumeration | Creation method. |
WeldJointBuilderWeldTypes Enumeration | Weld types. |
WeldLabelBuilderOrientationPlaneType Enumeration | This represents the Orientation Plane Type. |
WeldMeasurementSizeMethod Enumeration | the size method for measurement |
WeldObjectBuilderCommandName Enumeration | Commands that a callback will be invoked after dialog completion. |
WeldOverlapStatus Enumeration | the create status for overlap |
WeldParasetLocation Enumeration | the index of user picked refsheet location |
WeldPmiBuilderOrientationPlaneType Enumeration | This represents the Orientation Plane Type. |
WeldPointDirection Enumeration | Spot direction |
WeldPointExitBuilderCommandName Enumeration | The command name used for the newly created features. |
WeldPointExitBuilderMethodUsed Enumeration | The method use to create the features. |
WeldPointExtendMethod Enumeration | Offset curve extend method |
WeldPointLocation Enumeration | Settings locating spot welds using guide curves/edges |
WeldPointMethod Enumeration | Settings for method |
WeldPointReferenceSheetType Enumeration | Settings for the reference sheet |
WeldPointSpacingMethod Enumeration | Guide spacing method |
WeldPrepareEdges Enumeration | Settings for prepare edges |
WeldProjectionMethod Enumeration | Settings project method type |
WeldRootUpdate Enumeration | Arc process type |
WeldSelectionType Enumeration | the type of selction |
WeldSpacingCalcMethod Enumeration | Settings spacing method type |
WeldTaperMethod Enumeration | Settings for groove taper method |
Structs¶
JointExitBuilderFilletSizes_Struct Struct | The structure for defining fillet weld lengths. |
LogInfo Struct | Represents entity and its log message |
WeldJointBuilderJointMidPointData_Struct Struct | Joint evaluation information at the mid point. |
WeldObjectBuilderFeatureInfo_Struct Struct |
|
WeldPointExitBuilderFeatureInfo_Struct Struct |
|