WeldAdvisorCustomerDefault Enumeration¶
-
class
NXOpen.Weld.
WeldAdvisorCustomerDefault
¶ Bases:
object
the customer default value types Enum Members
Enum Member Enum Member Description ResistanceSpot Resistance SpotArcSpot Arc SpotClinch ClinchDollop DollopWeldNut Weld NutWeldStud Weld StudCustom1Point Custom1 PointCustom2Point Custom2 PointCustom3Point Custom3 PointCustom4Point Custom4 PointCustom5Point Custom5 PointDatum datum, used for implementing weld advisor parametersMeasurement measurement, used for implementing weld advisor parametersNum number of types-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-