ConnectedFaceFinderBuilder Class¶
-
class
NXOpen.Weld.
ConnectedFaceFinderBuilder
¶ Bases:
NXOpen.Builder
Represents a builder to run the Connected Face Finder operation.
To create a new instance of this class, use
NXOpen.Weld.WeldManager.CreateConnectedFaceFinderBuilder
Default values.
Property Value ConnectionFinder.Filter All ConnectionFinder.ListFeatureSet 1 ConnectionFinder.UpdateCoordinateSystem 1 New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
ConnectionFinder | Returns the connection finder object that manages the interaction. |
ListFeatureSet | Returns or sets the option if set to true will list the search results according to the feature sets that the specified weld point belongs to. |
RetainedWelds | Returns the retained weld objects that need to be reconnected. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
PerformAnalysis | Process the selected retained welds and populate the list with appropriate faces to reconnect the weld too. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ConnectionFinder¶
-
ConnectedFaceFinderBuilder.
ConnectionFinder
¶ Returns the connection finder object that manages the interaction.
-------------------------------------
Getter Method
Signature
ConnectionFinder()
Returns: Return type: NXOpen.Weld.ConnectionFinderBuilder
New in version NX9.0.0.
License requirements: None.
ListFeatureSet¶
-
ConnectedFaceFinderBuilder.
ListFeatureSet
¶ Returns or sets the option if set to true will list the search results according to the feature sets that the specified weld point belongs to.
-------------------------------------
Getter Method
Signature
ListFeatureSet()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ListFeatureSet(listFeatureSet)
Parameters: listFeatureSet (bool) – New in version NX9.0.0.
License requirements: ugweld (“UG WELD”)
RetainedWelds¶
-
ConnectedFaceFinderBuilder.
RetainedWelds
¶ Returns the retained weld objects that need to be reconnected.
-------------------------------------
Getter Method
Signature
RetainedWelds()
Returns: Weld Feature tag. Return type: NXOpen.SelectTaggedObjectList
New in version NX9.0.0.
License requirements: None.
Method Detail¶
PerformAnalysis¶
-
ConnectedFaceFinderBuilder.
PerformAnalysis
¶ Process the selected retained welds and populate the list with appropriate faces to reconnect the weld too.
Signature
PerformAnalysis()
New in version NX9.0.0.
License requirements: ugweld (“UG WELD”)
Validate¶
-
ConnectedFaceFinderBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.