WeldFillStripBuilder Class¶
-
class
NXOpen.Weld.
WeldFillStripBuilder
¶ Bases:
NXOpen.Builder
A builder used to create or edit a single strip of the
NXOpen.Weld.WeldFillBuilder
.To create a new instance of this class, use
NXOpen.Weld.WeldFillBuilder.NewFillStrip
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Center | Returns the center of the fill strip. |
Length | Returns or sets the length of the fill strip. |
Tag | Returns the Tag for this object. |
ToBeDeleted | Returns or sets the flag indicating that the strip should be deleted. |
Methods¶
Method | Description |
---|---|
AlignNegative | Aligns the end of the fill strip, opposite of the length direction from center, to the same end of the input fill strip. |
AlignPositive | Aligns the end of the fill strip, along the length direction from center, to the same end of the input fill strip. |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
JoinNegative | Joins the end of the fill strip, opposite of the length direction from center, to the other fill strip input. |
JoinPositive | Joins the end of the fill strip, along the length direction from center, to the other fill strip input. |
MoveDelta | Moves the fill strip the input length and width values. |
MoveToPoint | Moves the fill strip to the input center. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Split | Splits the fill strip at the center and creates a new strip. |
StretchNegative | Stretches the fill strip the input length opposite of the length direction. |
StretchPositive | Stretches the fill strip the input length in the length direction. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Center¶
-
WeldFillStripBuilder.
Center
¶ Returns the center of the fill strip.
-------------------------------------
Getter Method
Signature
Center()
Returns: Return type: NXOpen.Point3d
New in version NX7.5.0.
License requirements: None.
Length¶
-
WeldFillStripBuilder.
Length
¶ Returns or sets the length of the fill strip.
-------------------------------------
Getter Method
Signature
Length()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Length(length)
Parameters: length (float) – New in version NX7.5.0.
License requirements: None.
ToBeDeleted¶
-
WeldFillStripBuilder.
ToBeDeleted
¶ Returns or sets the flag indicating that the strip should be deleted.
-------------------------------------
Getter Method
Signature
ToBeDeleted()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToBeDeleted(flag)
Parameters: flag (bool) – New in version NX7.5.0.
License requirements: None.
Method Detail¶
AlignNegative¶
-
WeldFillStripBuilder.
AlignNegative
¶ Aligns the end of the fill strip, opposite of the length direction from center, to the same end of the input fill strip.
Signature
AlignNegative(alignStrip)
Parameters: alignStrip ( NXOpen.Weld.WeldFillStripBuilder
) – Fill strip to align to.New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
AlignPositive¶
-
WeldFillStripBuilder.
AlignPositive
¶ Aligns the end of the fill strip, along the length direction from center, to the same end of the input fill strip.
Signature
AlignPositive(alignStrip)
Parameters: alignStrip ( NXOpen.Weld.WeldFillStripBuilder
) – Fill strip to align to.New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
JoinNegative¶
-
WeldFillStripBuilder.
JoinNegative
¶ Joins the end of the fill strip, opposite of the length direction from center, to the other fill strip input.
Note the caller must delete the joinStrip if desired.
Signature
JoinNegative(joinStrip)
Parameters: joinStrip ( NXOpen.Weld.WeldFillStripBuilder
) – Fill strip to join with.New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
JoinPositive¶
-
WeldFillStripBuilder.
JoinPositive
¶ Joins the end of the fill strip, along the length direction from center, to the other fill strip input.
Note the caller must delete the joinStrip if desired.
Signature
JoinPositive(joinStrip)
Parameters: joinStrip ( NXOpen.Weld.WeldFillStripBuilder
) – Fill strip to join with.New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
MoveDelta¶
-
WeldFillStripBuilder.
MoveDelta
¶ Moves the fill strip the input length and width values.
Signature
MoveDelta(lengthDelta, widthDelta)
Parameters: - lengthDelta (float) – Distance to move strip in the length direction.
- widthDelta (float) – Distance to move strip in the width direction.
New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
MoveToPoint¶
-
WeldFillStripBuilder.
MoveToPoint
¶ Moves the fill strip to the input center.
Signature
MoveToPoint(newCenter)
Parameters: newCenter ( NXOpen.Point3d
) – New center of the fill stripNew in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
Split¶
-
WeldFillStripBuilder.
Split
¶ Splits the fill strip at the center and creates a new strip.
Signature
Split()
Returns: Return type: NXOpen.Weld.WeldFillStripBuilder
New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
StretchNegative¶
-
WeldFillStripBuilder.
StretchNegative
¶ Stretches the fill strip the input length opposite of the length direction.
Signature
StretchNegative(lengthDelta)
Parameters: lengthDelta (float) – Distance to stretch the strip opposite of the length direction. New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
StretchPositive¶
-
WeldFillStripBuilder.
StretchPositive
¶ Stretches the fill strip the input length in the length direction.
Signature
StretchPositive(lengthDelta)
Parameters: lengthDelta (float) – Distance to stretch the strip in the length direction. New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
Validate¶
-
WeldFillStripBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.