WeldFillBuilderBoundaryMethodType Enumeration¶
NXOpen.Weld.WeldFillBuilder.BoundaryMethodType is an alias for NXOpen.Weld.WeldFillBuilderBoundaryMethodType
-
class
NXOpen.Weld.
WeldFillBuilderBoundaryMethodType
¶ Bases:
object
Defines whether the initial boundary of the fill pattern is defined by a two point rectangle or a curve.
Enum Members
Enum Member Enum Member Description Rectangle Boundary defined by a two point rectangle.Curve Boundary defined by a curve.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-