EasyPatternBuilderSpacingMethodTypes Enumeration¶
NXOpen.Weld.EasyPatternBuilder.SpacingMethodTypes is an alias for NXOpen.Weld.EasyPatternBuilderSpacingMethodTypes
-
class
NXOpen.Weld.
EasyPatternBuilderSpacingMethodTypes
¶ Bases:
object
Indicates whether planes should be cut a grid lines, or if a single plane should be used.
Enum Members
Enum Member Enum Member Description Grid Use Grid spacing to cut sections.SinglePlane Use a single plane to cut a sections.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-