EdgePrepBuilder Class¶
-
class
NXOpen.Weld.
EdgePrepBuilder
¶ Bases:
NXOpen.Builder
A builder used to create or edit a
NXOpen.Weld.EdgePrep
feature.To create a new instance of this class, use
NXOpen.Weld.WeldManager.CreateEdgePrepBuilder
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
ErrorCode | Returns the error code for the first welding joint curve that could not be processed. |
Tag | Returns the Tag for this object. |
WeldObjects | Returns the welding joints to drive edge preparation |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetNoResultsInfo | Returns the curves that weld preparation was attempted on, but could not be performed. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ErrorCode¶
-
EdgePrepBuilder.
ErrorCode
¶ Returns the error code for the first welding joint curve that could not be processed.
-------------------------------------
Getter Method
Signature
ErrorCode()
Returns: Return type: int New in version NX8.5.0.
License requirements: None.
WeldObjects¶
-
EdgePrepBuilder.
WeldObjects
¶ Returns the welding joints to drive edge preparation
-------------------------------------
Getter Method
Signature
WeldObjects()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX8.0.0.
License requirements: None.
Method Detail¶
GetNoResultsInfo¶
-
EdgePrepBuilder.
GetNoResultsInfo
¶ Returns the curves that weld preparation was attempted on, but could not be performed.
Signature
GetNoResultsInfo()
Returns: The welding joint curves that weld preparation failed on. Return type: list of NXOpen.Curve
New in version NX8.5.0.
License requirements: None.
Validate¶
-
EdgePrepBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.