CharacteristicsValueBuilderType Enumeration¶
NXOpen.Weld.CharacteristicsValueBuilder.Type is an alias for NXOpen.Weld.CharacteristicsValueBuilderType
-
class
NXOpen.Weld.
CharacteristicsValueBuilderType
¶ Bases:
object
Settings to indicate the type of value contained in the attribute.
Enum Members
Enum Member Enum Member Description String Indicates the attribute value contains a string.Integer Indicates the attribute value contains a integer.Double Indicates the attribute value contains a double.Option Indicates the attribute value contains a pre set list of strings.None Indicates there is no attribute value.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-