JointmarkBuilderMethod Enumeration¶
NXOpen.Weld.JointmarkBuilder.Method is an alias for NXOpen.Weld.JointmarkBuilderMethod
-
class
NXOpen.Weld.
JointmarkBuilderMethod
¶ Bases:
object
The type of construction method for creating Jointmark
Enum Members
Enum Member Enum Member Description GuideCurve Guide CurveMirror MirrorPoints PointsTranslate TranslateExistingPoints Existing Points. Only allowed forNXOpen.Weld.PointMark
class.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-