WeldImportBuilder Class¶
-
class
NXOpen.Weld.
WeldImportBuilder
¶ Bases:
NXOpen.Builder
Creates Weld features by reading a csv file
To create a new instance of this class, use
NXOpen.Weld.WeldManager.CreateImportBuilder
New in version NX7.5.1.
Properties¶
Property | Description |
---|---|
ConfirmWarningMessages | Returns or sets the option to indicate if warning messages need to be confirmed. |
InputFile | Returns or sets the input csv file |
Tag | Returns the Tag for this object. |
TemplateFile | Returns or sets the template file indicating attribute mapping. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ConfirmWarningMessages¶
-
WeldImportBuilder.
ConfirmWarningMessages
¶ Returns or sets the option to indicate if warning messages need to be confirmed.
If false setting, all warnings will be accepted.
-------------------------------------
Getter Method
Signature
ConfirmWarningMessages()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConfirmWarningMessages(option)
Parameters: option (bool) – New in version NX8.5.0.
License requirements: structure_weld (“STRUCTURE WELD”)
InputFile¶
-
WeldImportBuilder.
InputFile
¶ Returns or sets the input csv file
-------------------------------------
Getter Method
Signature
InputFile()
Returns: Return type: str New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
InputFile(filename)
Parameters: filename (str) – New in version NX7.5.1.
License requirements: None.
TemplateFile¶
-
WeldImportBuilder.
TemplateFile
¶ Returns or sets the template file indicating attribute mapping.
-------------------------------------
Getter Method
Signature
TemplateFile()
Returns: Return type: str New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
TemplateFile(filename)
Parameters: filename (str) – New in version NX7.5.1.
License requirements: None.
Method Detail¶
Validate¶
-
WeldImportBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.