EasyPatternBuilderTypes Enumeration¶
NXOpen.Weld.EasyPatternBuilder.Types is an alias for NXOpen.Weld.EasyPatternBuilderTypes
-
class
NXOpen.Weld.
EasyPatternBuilderTypes
¶ Bases:
object
Controls the type of pattern.
Enum Members
Enum Member Enum Member Description TrimAndSurface Trim vector and surface vectors.HemAndSurface Hem vector and surface vectors.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-