WeldBeadBuilderTypes Enumeration¶
NXOpen.Weld.WeldBeadBuilder.Types is an alias for NXOpen.Weld.WeldBeadBuilderTypes
-
class
NXOpen.Weld.
WeldBeadBuilderTypes
¶ Bases:
object
Settings to indicate the sweep shape of the bead.
Enum Members
Enum Member Enum Member Description Ellipse ellipse shapeTube tube shapeSketch sketch shape-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-