JointmarkPointsBuilder Class¶
-
class
NXOpen.Weld.
JointmarkPointsBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Used to create or edit a point in the list of points for Jointmark
To create a new instance of this class, use
NXOpen.Weld.JointmarkBuilder.NewPoints
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
Angle | Returns the angle through which X and Y axis to rotate |
FlipDirection | Returns or sets the flip of Z axis. |
MappingFeature | Returns the selected feature to move to the location specified. |
Point | Returns or sets the point at which the feature is created |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
UpdateCsys | Update the csys using a new matrix. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
JointmarkPointsBuilderPointPosition Enumeration | The point classification |
Property Detail¶
Angle¶
-
JointmarkPointsBuilder.
Angle
¶ Returns the angle through which X and Y axis to rotate
-------------------------------------
Getter Method
Signature
Angle()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ugweld (“UG WELD”)
FlipDirection¶
-
JointmarkPointsBuilder.
FlipDirection
¶ Returns or sets the flip of Z axis.
Z axis representing the normal can be flipped
-------------------------------------
Getter Method
Signature
FlipDirection()
Returns: Return type: bool New in version NX9.0.0.
License requirements: ugweld (“UG WELD”)
-------------------------------------
Setter Method
Signature
FlipDirection(flip)
Parameters: flip (bool) – New in version NX9.0.0.
License requirements: ugweld (“UG WELD”)
MappingFeature¶
-
JointmarkPointsBuilder.
MappingFeature
¶ Returns the selected feature to move to the location specified.
-------------------------------------
Getter Method
Signature
MappingFeature()
Returns: Return type: NXOpen.Features.SelectFeature
New in version NX10.0.0.
License requirements: ugweld (“UG WELD”)
Point¶
-
JointmarkPointsBuilder.
Point
¶ Returns or sets the point at which the feature is created
-------------------------------------
Getter Method
Signature
Point()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: ugweld (“UG WELD”)
-------------------------------------
Setter Method
Signature
Point(point)
Parameters: point ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: ugweld (“UG WELD”)
Method Detail¶
UpdateCsys¶
-
JointmarkPointsBuilder.
UpdateCsys
¶ Update the csys using a new matrix.
Signature
UpdateCsys(matrix)
Parameters: matrix ( NXOpen.Matrix3x3
) – rotate matrixNew in version NX10.0.0.
License requirements: ugweld (“UG WELD”)
Validate¶
-
JointmarkPointsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.