WeldObjectBuilder Class¶
-
class
NXOpen.Weld.
WeldObjectBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Weld.WeldObjectBuilder
class used to collect welding objects created or edited from a command.New in version NX8.0.1.
Properties¶
Property | Description |
---|---|
CommandUsed | Returns the command name that was last used to create or modify features |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetFeatureInformation | Gets the created and modifed features |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
WeldObjectBuilderCommandName Enumeration | Commands that a callback will be invoked after dialog completion. |
Structs¶
WeldObjectBuilderFeatureInfo_Struct Struct |
|
Property Detail¶
CommandUsed¶
-
WeldObjectBuilder.
CommandUsed
¶ Returns the command name that was last used to create or modify features
-------------------------------------
Getter Method
Signature
CommandUsed()
Returns: command name used Return type: NXOpen.Weld.WeldObjectBuilderCommandName
New in version NX8.0.1.
License requirements: ugweld (“UG WELD”)
Method Detail¶
GetFeatureInformation¶
-
WeldObjectBuilder.
GetFeatureInformation
¶ Gets the created and modifed features
Signature
GetFeatureInformation()
Returns: features created or edited Return type: list of NXOpen.Weld.WeldObjectBuilderFeatureInfo_Struct
New in version NX8.0.1.
License requirements: ugweld (“UG WELD”)
Validate¶
-
WeldObjectBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.