JointExitBuilderFilletSizes_Struct Struct¶
NXOpen.Weld.JointExitBuilder.FilletSizes is an alias for NXOpen.Weld.JointExitBuilderFilletSizes_Struct
-
class
NXOpen.Weld.
JointExitBuilderFilletSizes_Struct
¶ Bases:
object
The structure for defining fillet weld lengths.
Fields¶
Field | Description |
---|---|
ThroatThickness | The fillet weld throat thickness |
LegLength1 | The fillet weld first length. |
LegLength2 | The fillet weld second length. |
ThroatThickness¶
-
JointExitBuilderFilletSizes_Struct.
ThroatThickness
¶ The fillet weld throat thickness
-------------------------------------
Getter Method Signature
ThroatThickness()
Returns: Return type: float -------------------------------------
Setter Method
Signature
ThroatThickness(value)
Parameters: value (float) –