JointItemBuilder Class

class NXOpen.Weld.JointItemBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Used to create or edit a Weld.WeldJoint feature.

To create a new instance of this class, use NXOpen.Weld.WeldJointBuilder.NewItem

New in version NX8.0.0.

Properties

Property Description
BackingFace Returns the backing face.
Curve Returns the joint curve
Limits Returns the limits of the joint curve span.
MasterEdge Returns the master edge of a T-joint weld.
PlacementFace Returns the placement face of a T-joint weld.
PrimaryEdge Returns the primary edge of a butt weld.
PrimaryFace Returns the primary face of a butt weld.
RoutingObject Returns the routing port.
SecondaryEdge Returns the secondary edge of a butt weld.
SecondaryFace Returns the secondary face of a butt weld.
Tag Returns the Tag for this object.
TargetFace Returns the target face of a T-joint weld.
UseCallbackValues Returns or sets the indication to use the values of the callback to define the joint
WeldType Returns or sets the weld type
WeldingCharacteristics Returns the collection of welding characteristics defined by attributes.

Methods

Method Description
DeleteCurve Deletes the joint curve from the builder.
ReadEdgePrepValues Read edge prep values set by the user plugin function.
SaveEdgePrepValues Save edge prep values to the Welding Joint.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

BackingFace

JointItemBuilder.BackingFace

Returns the backing face.

-------------------------------------

Getter Method

Signature BackingFace()

Returns:
Return type:NXOpen.ScCollector

New in version NX9.0.0.

License requirements: None.

Curve

JointItemBuilder.Curve

Returns the joint curve

-------------------------------------

Getter Method

Signature Curve()

Returns:
Return type:NXOpen.Curve

New in version NX8.5.0.

License requirements: None.

Limits

JointItemBuilder.Limits

Returns the limits of the joint curve span.

-------------------------------------

Getter Method

Signature Limits()

Returns:
Return type:NXOpen.Die.DieLimitsBuilder

New in version NX8.0.0.

License requirements: None.

MasterEdge

JointItemBuilder.MasterEdge

Returns the master edge of a T-joint weld.

-------------------------------------

Getter Method

Signature MasterEdge()

Returns:
Return type:NXOpen.ScCollector

New in version NX8.0.0.

License requirements: None.

PlacementFace

JointItemBuilder.PlacementFace

Returns the placement face of a T-joint weld.

For example, on a profile it is the face that touches the plate.

-------------------------------------

Getter Method

Signature PlacementFace()

Returns:
Return type:NXOpen.ScCollector

New in version NX8.0.0.

License requirements: None.

PrimaryEdge

JointItemBuilder.PrimaryEdge

Returns the primary edge of a butt weld.

-------------------------------------

Getter Method

Signature PrimaryEdge()

Returns:
Return type:NXOpen.ScCollector

New in version NX8.0.0.

License requirements: None.

PrimaryFace

JointItemBuilder.PrimaryFace

Returns the primary face of a butt weld.

-------------------------------------

Getter Method

Signature PrimaryFace()

Returns:
Return type:NXOpen.ScCollector

New in version NX8.0.0.

License requirements: None.

RoutingObject

JointItemBuilder.RoutingObject

Returns the routing port.

-------------------------------------

Getter Method

Signature RoutingObject()

Returns:
Return type:NXOpen.Routing.SelectPort

New in version NX10.0.0.

License requirements: None.

SecondaryEdge

JointItemBuilder.SecondaryEdge

Returns the secondary edge of a butt weld.

-------------------------------------

Getter Method

Signature SecondaryEdge()

Returns:
Return type:NXOpen.ScCollector

New in version NX8.0.0.

License requirements: None.

SecondaryFace

JointItemBuilder.SecondaryFace

Returns the secondary face of a butt weld.

-------------------------------------

Getter Method

Signature SecondaryFace()

Returns:
Return type:NXOpen.ScCollector

New in version NX8.0.0.

License requirements: None.

TargetFace

JointItemBuilder.TargetFace

Returns the target face of a T-joint weld.

For example, the plate face that the profile lies on.

-------------------------------------

Getter Method

Signature TargetFace()

Returns:
Return type:NXOpen.ScCollector

New in version NX8.0.0.

License requirements: None.

UseCallbackValues

JointItemBuilder.UseCallbackValues

Returns or sets the indication to use the values of the callback to define the joint

-------------------------------------

Getter Method

Signature UseCallbackValues()

Returns:
Return type:bool

New in version NX8.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature UseCallbackValues(status)

Parameters:status (bool) –

New in version NX8.0.0.

License requirements: structure_weld (“STRUCTURE WELD”)

WeldType

JointItemBuilder.WeldType

Returns or sets the weld type

-------------------------------------

Getter Method

Signature WeldType()

Returns:
Return type:int

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature WeldType(type)

Parameters:type (int) –

New in version NX8.5.0.

License requirements: structure_weld (“STRUCTURE WELD”)

WeldingCharacteristics

JointItemBuilder.WeldingCharacteristics

Returns the collection of welding characteristics defined by attributes.

-------------------------------------

Getter Method

Signature WeldingCharacteristics()

Returns:
Return type:NXOpen.Weld.CharacteristicsBuilder

New in version NX8.0.0.

License requirements: None.

Method Detail

DeleteCurve

JointItemBuilder.DeleteCurve

Deletes the joint curve from the builder.

Signature DeleteCurve()

New in version NX8.0.0.

License requirements: None.

ReadEdgePrepValues

JointItemBuilder.ReadEdgePrepValues

Read edge prep values set by the user plugin function.

Signature ReadEdgePrepValues()

Returns:
Return type:NXOpen.Weld.EdgePrepValuesBuilder

New in version NX8.0.0.

License requirements: structure_weld (“STRUCTURE WELD”)

SaveEdgePrepValues

JointItemBuilder.SaveEdgePrepValues

Save edge prep values to the Welding Joint.

Signature SaveEdgePrepValues(valuesBuilder)

Parameters:valuesBuilder (NXOpen.Weld.EdgePrepValuesBuilder) –

New in version NX8.0.0.

License requirements: structure_weld (“STRUCTURE WELD”)

Validate

JointItemBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.