CharacteristicsBuilderType Enumeration¶
NXOpen.Weld.CharacteristicsBuilder.Type is an alias for NXOpen.Weld.CharacteristicsBuilderType
-
class
NXOpen.Weld.
CharacteristicsBuilderType
¶ Bases:
object
The custom type of the datum specified for creation.
Enum Members
Enum Member Enum Member Description None FilletFeature GrooveFeature ResistanceSpotFeature ArcSpotFeature ClinchFeature DollopFeature WeldNutFeature WeldStudFeature Custom1PointFeature Custom2PointFeature Custom3PointFeature Custom4PointFeature Custom5PointFeature DatumSurfaceFeature DatumPinFeature DatumCustom1Feature DatumCustom2Feature DatumCustom3Feature MeasurementSurfaceFeature MeasurementHoleFeature MeasurementSlotFeature MeasurementStudFeature MeasurementTrimFeature MeasurementHemFeature MeasurementCustom1Feature MeasurementCustom2Feature MeasurementCustom3Feature UserDefinedFeature SealerFillFeature SealerBeadFeature JointFeature PlugSlotFeature ShipHull ShipDeck ShipTransverseBulkhead ShipLongitudinalBulkhead ShipGenericPlate ShipStiffener ShipEdgeReinforcement ShipSeam DatumSurfaceCustom0 DatumSurfaceCustom1 DatumSurfaceCustom2 DatumSurfaceCustom3 DatumSurfaceCustom4 DatumSurfaceCustom5 DatumSurfaceCustom6 DatumSurfaceCustom7 DatumPinCustom0 DatumPinCustom1 DatumPinCustom2 DatumPinCustom3 DatumPinCustom4 DatumPinCustom5 DatumPinCustom6 DatumPinCustom7 SurfaceWeld ShipProfileCutOut JointmarkFeature ShipStandardPart PointMarkResistanceSpot PointMarkArcSpot PointMarkDollop PointMarkClinch PointMarkWeldNut PointMarkWeldStud PointMarkCustom1 PointMarkCustom2 PointMarkCustom3 PointMarkCustom4 PointMarkCustom5 -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-