WeldJointBuilderDestinationTypes Enumeration¶
NXOpen.Weld.WeldJointBuilder.DestinationTypes is an alias for NXOpen.Weld.WeldJointBuilderDestinationTypes
-
class
NXOpen.Weld.
WeldJointBuilderDestinationTypes
¶ Bases:
object
Where to create new joints.
Enum Members
Enum Member Enum Member Description WorkPart Create new joints in work part.NewComponent Create a new componenent for each joint under the work part.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-