EasyPatternBuilder Class¶
-
class
NXOpen.Weld.
EasyPatternBuilder
¶ Bases:
NXOpen.Builder
Represents the easy pattern builder.
This is used to create hem, trim and surface measurement points at various plane locations. To create a new instance of this class, use
NXOpen.Weld.WeldManager.CreateEasyPatternBuilder
Default values.
Property Value BackEdgeOffset 2 (millimeters part), 0.08 (inches part) GridAngleTolerance 15 GridIncrement 25 (millimeters part), 1.0 (inches part) Height 25 (millimeters part), 1.0 (inches part) HemMethod MidPoint LengthAndWidth 5 (millimeters part), 0.02 (inches part) MaximumSpacing 20 (millimeters part), 0.8 (inches part) MinimumFlangeWidth 6.0 (millimeters part), 0.25 (inches part) NumberSurfaceVectors 1 PlaneLocation 0 PlaneMethod InferPlanes SpacingMethod Grid TrimEdgeOffset 2 (millimeters part), 0.08 (inches part) New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
BackEdgeOffset | Returns or sets the back edge offset. |
DistanceTolerance | Returns or sets the distance tolerance. |
GridAngleTolerance | Returns or sets the grid angle tolerance. |
GridIncrement | Returns or sets the grid increment. |
Height | Returns or sets the height of the measurement solid to create. |
HemMethod | Returns or sets the hem method. |
LengthAndWidth | Returns or sets the length and width of the measurement solid to create. |
MaximumSpacing | Returns or sets the maximum spacing between the trim edge offset and the back edge offset. |
MinimumFlangeWidth | Returns or sets the value used to control when only one surface measurement vector will be created. |
NumberSurfaceVectors | Returns or sets the number surface vectors to create for each pattern. |
PatternPath | Returns the pattern path. |
PlaneLocation | Returns or sets the plane location. |
PlaneMethod | Returns or sets the plane method. |
ReverseDirection | Returns or sets the reverse direction. |
SpacingMethod | Returns or sets the spacing method. |
SurfaceVectorFace | Returns the surface vector face. |
Tag | Returns the Tag for this object. |
TrimEdgeOffset | Returns or sets the trim edge offset distance. |
Type | Returns or sets the type of pattern to created. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
EasyPatternBuilderHemMethodTypes Enumeration | Indicates the method to use to compute the hem vector location. |
EasyPatternBuilderPlaneMethodTypes Enumeration | The plane to cut sections in to determine placement measurement patterns. |
EasyPatternBuilderSpacingMethodTypes Enumeration | Indicates whether planes should be cut a grid lines, or if a single plane should be used. |
EasyPatternBuilderTypes Enumeration | Controls the type of pattern. |
Property Detail¶
BackEdgeOffset¶
-
EasyPatternBuilder.
BackEdgeOffset
¶ Returns or sets the back edge offset.
This offset distance is measured from the end of the section cut curve. The start of the curve is at path curve specified.
-------------------------------------
Getter Method
Signature
BackEdgeOffset()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BackEdgeOffset(backEdgeOffset)
Parameters: backEdgeOffset (float) – New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
DistanceTolerance¶
-
EasyPatternBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance.
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance(tolerance)
Parameters: tolerance (float) – New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
GridAngleTolerance¶
-
EasyPatternBuilder.
GridAngleTolerance
¶ Returns or sets the grid angle tolerance.
This is used for the inferred grid spacing method.
-------------------------------------
Getter Method
Signature
GridAngleTolerance()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GridAngleTolerance(gridAngleTolerance)
Parameters: gridAngleTolerance (float) – New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
GridIncrement¶
-
EasyPatternBuilder.
GridIncrement
¶ Returns or sets the grid increment.
The grid spacing value use to generate planes.
-------------------------------------
Getter Method
Signature
GridIncrement()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GridIncrement(gridIncrement)
Parameters: gridIncrement (float) – New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
Height¶
-
EasyPatternBuilder.
Height
¶ Returns or sets the height of the measurement solid to create.
-------------------------------------
Getter Method
Signature
Height()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Height(height)
Parameters: height (float) – New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
HemMethod¶
-
EasyPatternBuilder.
HemMethod
¶ Returns or sets the hem method.
This controls the method used for determining the hem point location and vector direction.
-------------------------------------
Getter Method
Signature
HemMethod()
Returns: Return type: NXOpen.Weld.EasyPatternBuilderHemMethodTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HemMethod(hemMethod)
Parameters: hemMethod ( NXOpen.Weld.EasyPatternBuilderHemMethodTypes
) –New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
LengthAndWidth¶
-
EasyPatternBuilder.
LengthAndWidth
¶ Returns or sets the length and width of the measurement solid to create.
-------------------------------------
Getter Method
Signature
LengthAndWidth()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LengthAndWidth(lengthAndWidth)
Parameters: lengthAndWidth (float) – New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
MaximumSpacing¶
-
EasyPatternBuilder.
MaximumSpacing
¶ Returns or sets the maximum spacing between the trim edge offset and the back edge offset.
-------------------------------------
Getter Method
Signature
MaximumSpacing()
Returns: Return type: float New in version NX7.5.5.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaximumSpacing(maximumSpacing)
Parameters: maximumSpacing (float) – New in version NX7.5.5.
License requirements: ugweld (“UG WELD”)
MinimumFlangeWidth¶
-
EasyPatternBuilder.
MinimumFlangeWidth
¶ Returns or sets the value used to control when only one surface measurement vector will be created.
-------------------------------------
Getter Method
Signature
MinimumFlangeWidth()
Returns: Return type: float New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
MinimumFlangeWidth(minimumFlangeWidth)
Parameters: minimumFlangeWidth (float) – New in version NX7.5.1.
License requirements: ugweld (“UG WELD”)
NumberSurfaceVectors¶
-
EasyPatternBuilder.
NumberSurfaceVectors
¶ Returns or sets the number surface vectors to create for each pattern.
-------------------------------------
Getter Method
Signature
NumberSurfaceVectors()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumberSurfaceVectors(numberSurfaceVectors)
Parameters: numberSurfaceVectors (int) – New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
PatternPath¶
-
EasyPatternBuilder.
PatternPath
¶ Returns the pattern path.
This path is used to determine the pattern spacing.
-------------------------------------
Getter Method
Signature
PatternPath()
Returns: Return type: NXOpen.Section
New in version NX7.5.0.
License requirements: None.
PlaneLocation¶
-
EasyPatternBuilder.
PlaneLocation
¶ Returns or sets the plane location.
The single plane location to create a pattern.
-------------------------------------
Getter Method
Signature
PlaneLocation()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlaneLocation(planeLocation)
Parameters: planeLocation (float) – New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
PlaneMethod¶
-
EasyPatternBuilder.
PlaneMethod
¶ Returns or sets the plane method.
This is used to control plane orientations for the measurement points.
-------------------------------------
Getter Method
Signature
PlaneMethod()
Returns: Return type: NXOpen.Weld.EasyPatternBuilderPlaneMethodTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlaneMethod(planeMethod)
Parameters: planeMethod ( NXOpen.Weld.EasyPatternBuilderPlaneMethodTypes
) –New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
ReverseDirection¶
-
EasyPatternBuilder.
ReverseDirection
¶ Returns or sets the reverse direction.
This will reverse direction of all measurement points created.
-------------------------------------
Getter Method
Signature
ReverseDirection()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseDirection(reverseDirection)
Parameters: reverseDirection (bool) – New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
SpacingMethod¶
-
EasyPatternBuilder.
SpacingMethod
¶ Returns or sets the spacing method.
This method controls whether multiple patterns are created or a single pattern.
-------------------------------------
Getter Method
Signature
SpacingMethod()
Returns: Return type: NXOpen.Weld.EasyPatternBuilderSpacingMethodTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SpacingMethod(spacingMethod)
Parameters: spacingMethod ( NXOpen.Weld.EasyPatternBuilderSpacingMethodTypes
) –New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
SurfaceVectorFace¶
-
EasyPatternBuilder.
SurfaceVectorFace
¶ Returns the surface vector face.
This is the face surface vectors will be created on.
-------------------------------------
Getter Method
Signature
SurfaceVectorFace()
Returns: Return type: NXOpen.ScCollector
New in version NX7.5.0.
License requirements: None.
TrimEdgeOffset¶
-
EasyPatternBuilder.
TrimEdgeOffset
¶ Returns or sets the trim edge offset distance.
This is the offset distance from the path specified.
-------------------------------------
Getter Method
Signature
TrimEdgeOffset()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TrimEdgeOffset(trimEdgeOffset)
Parameters: trimEdgeOffset (float) – New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
Type¶
-
EasyPatternBuilder.
Type
¶ Returns or sets the type of pattern to created.
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Weld.EasyPatternBuilderTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Weld.EasyPatternBuilderTypes
) –New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
Method Detail¶
Validate¶
-
EasyPatternBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.