JointmarkFaceSetsBuilder Class¶
-
class
NXOpen.Weld.
JointmarkFaceSetsBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Used to create or edit a set of faces for Jointmark
To create a new instance of this class, use
NXOpen.Weld.JointmarkBuilder.NewFaceSets
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
FaceSelect | Returns the selected face collector |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
FaceSelect¶
-
JointmarkFaceSetsBuilder.
FaceSelect
¶ Returns the selected face collector
-------------------------------------
Getter Method
Signature
FaceSelect()
Returns: Return type: NXOpen.ScCollector
New in version NX9.0.0.
License requirements: ugweld (“UG WELD”)
Method Detail¶
Validate¶
-
JointmarkFaceSetsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.