WeldPointExitBuilderMethodUsed Enumeration¶
NXOpen.Weld.WeldPointExitBuilder.MethodUsed is an alias for NXOpen.Weld.WeldPointExitBuilderMethodUsed
-
class
NXOpen.Weld.
WeldPointExitBuilderMethodUsed
¶ Bases:
object
The method use to create the features.
Enum Members
Enum Member Enum Member Description None No method specified. Used to initialize value.Mirror Feature was created using the mirror method.Translate Feature was created using the translate method.GuideCurve Feature was created using the guide curves method.Points Feature was created using the points method.GuideCurveMovedOff Feature was created using the guide curves method, but user moved it off.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-