Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
nxopen.cae.connections |
Provides classes and interfaces relating to Connections.
|
nxopen.cae.qualityaudit |
Provides classes and interfaces relating to Quality Audit.
|
Class and Description |
---|
ElementCollection
Element collection provides methods to manage
Element objects
To obtain an instance of this class, refer to BaseFEModel Created in NX11.0.0 |
Folder
The Folder class offers a way to create a hierarchy of connections and sub-folders
To obtain an instance of this object use the add_folder creator in a parent folder or access connection root folder from IFEModel Created in NX12.0.0 |
Class and Description |
---|
ComponentData
Composer connection.
|
ComposerConnectionType
composer Connection type
|
ComposerData
Composer connection.
|
ConnectionData
Composer connection.
|
ConnectionDBData
Connection DB data.
|
ConnectionDBItemData
Connection DB item data.
|
ConnectionDBItemStiffnessType
connection DB item stiffness type
|
ConnectionType
Connection type
|
CoordinatesLocation
Location interface.
|
CoordinatesSeriesLocation
Location interface.
|
CsysType
Csys types
|
CurveLocation
Location interface.
|
DiameterType
Diameter definition types
|
Dof
Degrees of freedom definition
|
DofCombination
Degrees Of Freedom Combination types
|
DofType
Degrees Of Freedom types
|
Element
This is the class to access a connection element
To obtain an instance of this object use the Create creator in ElementCollection . |
ElementStatusType
Element status
|
ElementType
Element type
|
FeEdgesLocation
Location interface.
|
Folder
The Folder class offers a way to create a hierarchy of connections and sub-folders
To obtain an instance of this object use the add_folder creator in a parent folder or access connection root folder from IFEModel Created in NX12.0.0 |
HeadDiameterType
Head diameter definition types
|
HeightType
Types of height definitions
|
IConnection
This class represents an interface to a connection object.
|
ICsys
This class represents an Interface to the Connection Csys.
|
IDiameter
This class represents an Interface to the Diameter parameters.
|
IDof
This class represents an interface to the connection's degrees of freedom.
|
IDofCombination
This class represents an interface to the connection's degrees of freedom combination.
|
IFlangesContainer
This interface offers access to the flanges of a connection (SpotWeld for example).
|
IHeight
This class represents an Interface to the Height parameters.
|
ILineDiscretization
This class represents an Interface to the Diameter parameters.
|
ILineOffset
This class represents an Interface to the Diameter parameters.
|
ILocationsContainer
This class represents an Interface to the Locations parameters.
|
ILocationsMultiPointContainer
This class represents an Interface to the Multi Point Locations container.
|
ILocationsSinglePointContainer
This class represents an Interface to the Locations parameters.
|
ILocationsWithDirContainer
This class represents an Interface to the Locations parameters.
|
ILocationsWithDiscretizationContainer
This class represents an Interface to the Locations With Discretization container.
|
IMaterial
This class represents an Interface to the Material entity.
|
INodalTargetCenter
This class represents an Interface to the Connection Target.
|
INodalTargetLegs
This class represents an Interface to the Connection Target.
|
INodalTargetsContainer
This class represents an Interface to the Connection Target Container.
|
INodalTargetsPairing
This class represents an Interface to the nodal connections pairing algorithm parameters.
|
IStiffness
This class represents an Interface to the Stiffness constants.
|
IStiffnessDynamic
This class represents an Interface to the Stiffness dynamic.
|
IStructuralDamping
This class represents an Interface to the StructuralDamping constants.
|
IStructuralDampingDynamic
This class represents an Interface to the StructuralDamping dynamic.
|
ITolerance
This class represents an Interface to the Tolerance parameters.
|
IViscousDamping
This class represents an Interface to the ViscousDamping constants.
|
IViscousDampingDynamic
This class represents an Interface to the ViscousDamping dynamic.
|
IWidth
This class represents an Interface to the Width parameters.
|
Location
Location base class.
|
LocationDirectionType
Location and Direction type
|
LocationType
Location type
|
LocationWithDir
Location With Direction interface.
|
MaterialType
Material definition types
|
ModelizationPPTRefTargetType
Modelization PPTRefTargetType
|
ModelizationResultType
Modelization result type
|
NodalPairingMethod
Nodal pairing method
|
NodalTarget
This class represents an Interface to the Connection Target.
|
NodalTargetType
Nodal Target types
|
NodeLocation
Location interface.
|
NodeSeriesLocation
Location interface.
|
PointLocation
Location interface.
|
PointSeriesLocation
Location interface.
|
SeamWeldMaterialType
Seam Weld Material type
|
SeamWeldType
Seam Weld Type
|
SelectionRecipeLocation
Location interface.
|
SpotWeld
Spot Weld connection.
|
TargetDependencyType
Nodal target dependency type
|
Utils
Contains universal connections utility methods
To obtain an instance of this class, refer to Folder Created in NX12.0.0 |
Class and Description |
---|
IConnection
This class represents an interface to a connection object.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.