See: Description
Interface | Description |
---|---|
Action |
The Quality Audit Action is a base class that performs actions on a list of objects.
|
ActionList |
The Quality Audit ActionList class offers means to select, deselect, obtain
Action instances. |
ActionSettings |
The Quality Audit ActionSettings is the base class for
Action settings. |
ComponentSynthesis |
This action has as result a list of components and the connections using them.
|
ConnectionDistanceCheck |
This action checks the distance between connections.
|
ConnectionDistanceResult |
The Quality Audit ConnectionPointsDistanceResult is a class containing information about failed distance between connection distance checks on universal connections.
|
ConnectionPointsDistanceCheck |
This action checks the distance between connection's definition points.
|
ConnectionPointsDistanceResult |
The Quality Audit ConnectionPointsDistanceResult is a class containing information about failed distance between connection points checks on universal connections.
|
ConnectivityCheck |
This action's output is a list of connected groups together with the involved connections.
|
DiameterCheck |
This action performs checks on connections supporting diameter and displays errors when diameter is different from the expected one.
|
DiameterResult |
The Quality Audit DiameterResult is a class containing information about failed diameter checks of universal connections.
|
FreeEdgeDistanceCheck |
This action checks if there are connections that are too close to the edge based on a configurable tolerance.
|
FreeEdgeDistanceResult |
The Quality Audit FreeEdgeDistanceResult contains information about problematic places where distance between connection points and free edges is less than a given value.
|
InputList |
The Quality Audit InputList class offers means to select, deselect, obtain the objects to be used by
Action instances. |
ListConnections |
This action has as result the list of all connections from the specified model.
|
ListConnectionsResult |
The Quality Audit ListConnectionsResult is a class containing information about connections found when performing the
ListConnections action. |
ListNonModeledConnections |
This action's output is a list of connections that are not realized.
|
ListNonModeledConnectionsResult |
This is a class containing information about the non modeled universal connections.
|
Manager |
The Quality Audit Manager class offers means to check for errors at assembly level
To obtain an instance of this class use CaeSession.qualityAuditManager() . |
ManualElementsResult |
The Quality Audit ManualElementsResult is a class containing information about nodes connecting components.
|
MergedNodesResult |
The Quality Audit MergedNodesResult is a class containing information about nodes connecting components.
|
MeshLevelFailedElementCreationResult |
The Quality Audit MeshLevelFailedElementCreationResult is a class containing information about failed element creations on universal connections.
|
MeshLevelFailedProjectionResult |
The Quality Audit MeshLevelFailedProjectionResult is a class containing information about failed projections on universal connections.
|
MeshLevelFailedProjectionToleranceResult |
The Quality Audit MeshLevelFailedProjectionToleranceResult is a class containing information about mesh projections
that failed the tolerance criteria.
|
MeshLevelProjectionCheck |
This action has as output the list of failed projections of the universal connections at mesh level.
|
MinimumDistanceSettings |
This class contains the minimum distance settings available for the following actions:
FreeEdgeDistanceCheck
ConnectionDistanceCheck
ConnectionPointsDistanceCheck
To obtain an instance of this class get the Action.settings() of classed using it. |
ObjectLevelCorrectedProjectionResult |
The Quality Audit ObjectLevelCorrectedProjectionResult is a class containing information about corrected projections on universal connections.
|
ObjectLevelFailedProjectionResult |
The Quality Audit ObjectLevelFailedProjectionResult is a class containing information about failed projections on universal connections.
|
ObjectLevelFailedProjectionToleranceResult |
The Quality Audit ObjectLevelFailedProjectionToleranceResult is a class containing information about projections
that failed the tolerance criteria although the projection itself was successful.
|
ObjectLevelProjectionCheck |
This action has as output the list of failed projections of the universal connections at object level.
|
ProjectionCheckSettings |
This class contains settings used by the projection checks.
|
Result |
The Quality Audit Result class offers means to access information about specific problems found while performing specific quality audit checks.
|
SupportSequenceCheck |
This action's output is the list of connections having more than 2 supports with wrong order (e.g. first support between the second and third).
|
Class | Description |
---|---|
Action.Id |
Action ids.
|
Manager.ActionType |
Action type to be used in the quality audit process.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.