See: Description
Interface | Description |
---|---|
BaseBuilder |
Represents the abstract builder class for all objects defined in response analysis meta solution
This is an abstract class, and cannot be created. |
CombinationEvaluationOptions |
Represents the setting for combination evaluation.
|
CsdEvaluationSetting |
Represents the class of evaluation setting for CSD
To create or edit an instance of this class, use CsdEvaluationSettingBuilder Created in NX6.0.0 |
CsdEvaluationSettingBuilder |
Represents the CSD build
To create a new instance of this class, use EvaluationSettingManager.createCsdEvaluationSettingBuilder(nxopen.cae.responsesimulation.CsdEvaluationSetting) Created in NX6.0.0 |
CSDExcitation |
Represents an CSD excitation.
|
CSDExcitationBuilder |
Represents the manager to
CSDExcitation . |
DataLocation |
Represents the data location to perform evaluation .
|
DDAMComponentData |
Represents an excitation on one specified direction.
|
DDAMExcitation |
Represents an DDAM excitation.
|
DDAMExcitationBuilder |
Represents the manager to
DDAMExcitation . |
DistributedLoadExcitation |
Represents an excitation of distributed-load type
To create or edit an instance of this class, use DistributedLoadExcitationBuilder Created in NX5.0.0 |
DistributedLoadExcitationBuilder |
Represents the manager to
DistributedLoadExcitation . |
DynamicEvaluationOutputSettings |
Represents the output setting for dynamic response evaluation .
|
DynamicResultEvaluationSetting |
Represents the abstract class of evaluation setting for all dynamic results evaluations.
|
DynamicResultEvaluationSettingBuilder |
Represents the abstract builder class of evaluation setting for all dynamic results evaluations.
|
ElementalFunctionEvaluationSetting |
Represents the parameters setting for elemental function evaluation.
|
ElementalFunctionEvaluationSettingBuilder |
This is a manager to the
ElementalFunctionEvaluationSetting class. |
EvaluationParameters |
Represents the evaluation parameters for a response simulation meta solution
Not support KF. |
EvaluationSetting |
Represents the abstract class of all evaluation setting classes.
|
EvaluationSettingBuilder |
Represents the abstract builder class of all evaluation setting classes.
|
EvaluationSettingManager |
Represents the manager of all evaluation setting objects.
|
Excitation |
Represents the abstract class of dynamic excitations
This is an abstract class, and cannot be created. |
ExcitationBuilder |
Represents the abstract excitation builder class.
|
ExcitationCollection |
Represents a collection of excitation objects
To obtain an instance of this class, refer to Manager Created in NX5.0.0 |
ExcitationLocationDefinition |
Represents the manager to
DistributedLoadExcitation . |
FrequencyDefinition |
Represents the frequency setting to perform FRF evaluation .
|
FrfEvaluationSetting |
Represents the parameters setting for FRF results evaluation
To create or edit an instance of this class, use FrfEvaluationSettingBuilder Created in NX5.0.0 |
FrfEvaluationSettingBuilder |
This is a manager to the
FrfEvaluationSetting class. |
FunctionComponentData |
Represents a function component setting of
NodalFunctionExcitation on one direction
Created in NX5.0.0 |
FunctionEvaluationOutputSettings |
Represents the output setting for function response evaluation .
|
FunctionEvaluationSetting |
Represents the abstract class of evaluation setting for function response evaluation
This is an abstract class, and cannot be created. |
FunctionEvaluationSettingBuilder |
Represents the abstract builder class of evaluation setting for function response evaluation
This is an abstract class, and cannot be created. |
InitialConditions |
Represents the initial condition setting of transient event .
|
LcrResultsEvaluationSetting |
Represents the parameters setting of LCR results evaluation.
|
LcrResultsEvaluationSettingBuilder |
This is a manager to the
LcrResultsEvaluationSetting class. |
Manager |
Represents the Response Dynamics manager to contain all Response Dynamics objects
To obtain an instance of this class, refer to SimSimulation Created in NX5.0.0 |
ModalProperties |
Represents the modal presentation of a response analysis meta solution .
|
ModalResultsEvaluationSetting |
Represents the abstract class of evaluation setting for FRF and transmissibility
This is an abstract class, and cannot be created. |
ModalResultsEvaluationSettingBuilder |
Represents the abstract builder class of evaluation setting for FRF and transmissibility
This is an abstract class, and cannot be created. |
ModeInitialData |
Represents the initial setting for a normal mode .
|
NodalFunctionEvaluationSetting |
Represents the parameters setting of nodal function response evaluation.
|
NodalFunctionEvaluationSettingBuilder |
This is a manager to the
NodalFunctionEvaluationSetting class. |
NodalFunctionExcitation |
Represents the abstract class of nodal function excitation
This is an abstract class, and cannot be created. |
NodalFunctionExcitationBuilder |
Represents the manager to
NodalFunctionExcitation . |
NormalMode |
Represents the properties of one normal mode .
|
ObjectLabel |
Represents the setting to label an object.
|
PeakValueEvaluationSetting |
Represents the parameters setting of peak value evaluation.
|
PeakValueEvaluationSettingBuilder |
This is a manager to the
PeakValueEvaluationSetting class. |
PhysicalDampingSettings |
Represents the physical damping settings for a response simulation meta solution .
|
PrlResultsEvaluationSetting |
Represents the abstract class of evaluation setting for peak value, RMS results
and LCR results.
|
PrlResultsEvaluationSettingBuilder |
Represents the abstract builder class of evaluation setting for peak value, RMS results
and LCR results.
|
ResponseResultsEvaluationSetting |
Represents the parameters setting for response results evaluation.
|
ResponseResultsEvaluationSettingBuilder |
This is a manager to the
ResponseResultsEvaluationSetting class. |
RmsResultsEvaluationSetting |
Represents the parameters setting for RMS results evaluation in response analysis.
|
RmsResultsEvaluationSettingBuilder |
This is a manager to the
RmsResultsEvaluationSetting class. |
RotationalDDAMExcitation |
Represents an DDAM excitation.
|
RotationalDDAMExcitationBuilder |
Represents the manager to
DDAMExcitation . |
RotationalNodalFunctionExcitation |
Represents a rotational nodal function excitation
To create or edit an instance of this class, use RotationalNodalFunctionExcitationBuilder Created in NX5.0.0 |
RotationalNodalFunctionExcitationBuilder |
Represents the manager to
RotationalNodalFunctionExcitation . |
RSDisplayObject |
Represents a BC display attributes
.
|
RSEvent |
Represents a response analysis event
To create or edit an instance of this class, use RSEventBuilder Created in NX5.0.0 |
RSEventAttributes |
Represents all possible attributes setting for response analysis event .
|
RSEventBuilder |
Represents the manager of CAE.ResponseSimulation.RSEvent.
|
RSEventCollection |
Represents a collection of response analysis event
To obtain an instance of this class, refer to Manager Created in NX5.0.0 |
RSEventOutputSetting |
Reprensents the output setting for an event .
|
RSEventSolverParameters |
Represents a response analysis event .
|
Sensor |
Represents a
Sensor
To create or edit an instance of this class, use SensorBuilder Created in NX5.0.0 |
SensorBuilder |
Represents a
SensorBuilder
To create a new instance of this class, use SensorCollection.createSensorBuilder(nxopen.cae.responsesimulation.Sensor) Created in NX5.0.0 |
SensorCollection |
Represents a collection of response analysis sensor
To obtain an instance of this class, refer to Manager Created in NX5.0.0 |
SensorEvaluationSetting |
Represents the parameters setting for sensor evaluation.
|
SensorEvaluationSettingBuilder |
This is a manager to the
SensorEvaluationSetting class. |
Solution |
Represents a meta solution providing response analysis functionalities in the .sim file
To create or edit an instance of this class, use SolutionBuilder Created in NX5.0.0 |
SolutionAttributes |
Represents attributes setting of response analysis meta solution .
|
SolutionBuilder |
This is a manager to the
Solution class. |
SolutionCollection |
Represents a collection of response analysis meta solution
To obtain an instance of this class, refer to Manager Created in NX5.0.0 |
StaticLoadExcitation |
Represents an excitation of static load type
To create or edit an instance of this class, use StaticLoadExcitationBuilder Created in NX6.0.0 |
StaticLoadExcitationBuilder |
Represents the manager to
StaticLoadExcitation . |
StrainGage |
Represents a
StrainGage
To create or edit an instance of this class, use StrainGageBuilder Created in NX6.0.0 |
StrainGageBuilder |
Represents a StrainGageBuilder
To create a new instance of this class, use StrainGageCollection.createStrainGageBuilder(nxopen.cae.responsesimulation.StrainGage) Default values. |
StrainGageCollection |
Represents a collection of response analysis strain gage
To obtain an instance of this class, refer to Manager Created in NX6.0.0 |
StrainGageEvaluationSetting |
Represents the parameters setting for strain gage evaluation.
|
StrainGageEvaluationSettingBuilder |
This is a manager to the
StrainGageEvaluationSetting class. |
StrengthResultsEvaluationSetting |
Represents parameters setting for strength results evaluation.
|
StrengthResultsEvaluationSettingBuilder |
This is a manager to the
StrengthResultsEvaluationSetting class. |
TranslationalDDAMExcitation |
Represents an DDAM excitation.
|
TranslationalDDAMExcitationBuilder |
Represents the manager to
DDAMExcitation . |
TranslationalNodalFunctionExcitation |
Represents a translational nodal function excitation
To create or edit an instance of this class, use TranslationalNodalFunctionExcitationBuilder Created in NX5.0.0 |
TranslationalNodalFunctionExcitationBuilder |
Represents the manager to
TranslationalNodalFunctionExcitation . |
TransmissibilityEvaluationSetting |
Represents parameters setting for transmissibility evaluation
To create or edit an instance of this class, use TransmissibilityEvaluationSettingBuilder Created in NX5.0.0 |
TransmissibilityEvaluationSettingBuilder |
This is a manager to the
TransmissibilityEvaluationSetting class. |
VelocityImpactDirection | |
VelocityImpactExcitation |
Represents a velocity impact excitation
To create or edit an instance of this class, use VelocityImpactExcitationBuilder Created in NX6.0.0 |
VelocityImpactExcitationBuilder |
Represents a
VelocityImpactExcitationBuilder
To create a new instance of this class, use ExcitationCollection.createVelocityImpactExcitationBuilder(nxopen.cae.responsesimulation.VelocityImpactExcitation) Default values. |
VelocityImpactParameters |
Class | Description |
---|---|
CombinationEvaluationOptions.EvaluationMethod |
Specifies the calculation method of combination evaluation
|
CombinationEvaluationOptions.MultipleExcitationCombinationMethod |
Specifies combination method for multiple excitation combination
|
CoordinateSystem |
Specifies the coordinate system
|
CSDExcitation.CorrelationType |
Represents the correlation type.
|
CSDExcitationBuilder.CSDFunction |
This class holds the data returned from
CSDExcitationBuilder.getFromFunction() |
DataLocation.Beam |
Specifies the location for beam
|
DataLocation.Element |
Specifies the element location for element
|
DataLocation.Shell |
Specifies the location for shell
|
DDAMComponentData.LoadingType |
Specifies the loading type
|
DDAMComponentData.ResponseType |
Specifies the response type
|
DDAMExcitation.CoefficientDefinitionType |
the choices of define DDAM coefficients.
|
DDAMExcitation.LoadingType |
Specifies the loading type
|
DDAMExcitation.MountingType |
Specifies the mounting type
|
DDAMExcitation.ResponseType |
Specifies the response type
|
DDAMExcitation.ShipType |
Specifies the ship type
|
DirectionDataComponent |
Specifies the direction data components
|
ElementalFunctionEvalBeamLocation |
Specifies beam element evaluation locations
|
ElementLocation |
Specifies element locations
|
EvaluationParameters.AnalysisIntegrationMethod |
the integration method used for transient analysis
|
EvaluationResultType |
Specifies the evaluation result type
|
Excitation.Component |
Represents the component type.
|
ExcitationBuilder.ExcitationLocationType |
the type of excitation location
|
FrequencyDefinition.Definition |
Specifies the method to define frequency
|
FrequencyDefinition.InterpolationMethod |
Specifies the method for interpolation
|
InitialConditions.EntryMethod |
Specifies how to define initial condition for the user customization
|
InitialConditions.Type |
Specifies the method to define initial condition
|
InterpolationMethod |
This enum defines interpolation method
|
NodalAveragingOption |
Specifies nodal averaging options
|
NodalFunctionEvalBeamLocation |
Specifies beam element evaluation locations for nodal function evaluation
|
NodalFunctionEvalRequest |
Specifies response request for nodal function evaluation
|
NodalFunctionEvalShellLocation |
Specifies shell element evaluation locations for nodal function evaluation
|
NodalFunctionExcitation.Type |
the subtype of nodal function excitation
|
ResponseDomainDefinitionMethod |
Specifies response result evaluation options
|
RmsLcrEvaluationMethod |
Specifies the evaluation method for RMS or LCR calculation
|
RSEvent.AnalysisType |
the analysis type of response analysis event.
|
RSEvent.DdamFormulationType |
Represents the fromulation type.
|
RSEvent.DurationOption |
the duration option
|
RSEvent.ResultFileType |
the result file type of event.
|
RSEvent.SpacingType |
the spacing type.
|
RSEvent.Type |
the type of reponse analysis event
|
RSEventSolverParameters.DdamCoefficientType |
Represents DDAM coefficient type
|
SensorCoordinateType |
Specifies the coordinate type of Sensor
|
SensorResultType |
Specifies the result type of Sensor
|
SensorType |
Specifies the type of Sensor
|
ShellElementEvaluationLocation |
Specifies shell element evaluation locations
|
StrainGageOrientationPlane |
Specifies the orientation plane type of Strain Gage
|
StrainGagePlacementType |
Specifies the placement type of Strain Gage
|
StrainGageResult |
Specifies the result type of Strain Gage
|
StrainGageShellElementFaceType |
Specifies the shell element location type of Strain Gage
|
StrainGageType |
Specifies the type of Strain Gage
|
StrengthStressCriteria |
Specifies strength stress criteria
|
StrengthStressMaterialDefinitionMethod |
Specifies the definition method for material
|
StrengthStressOption |
The options of stress
|
TranslationalNodalFunctionExcitationBuilder.RotationAxisType |
Represents the rotation axis type.
|
TransmissibilityEvaluationSettingBuilder.MotionType |
This enum defines input motion type
|
VelocityImpactDirection.DirectionType |
the direction options for impact
|
VelocityImpactDirection.NodalComponentType |
the types of nodal component
|
VelocityImpactExcitationBuilder.ImpactMethodType |
the impact definiton methods
|
VelocityImpactParameters.StartPositionType |
the calculation start position for impact
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.