Modifier and Type | Method and Description |
---|---|
AssociationUtilities |
associationUtils()
|
CaeDataContainer |
getDataContainer()
Returns a
CaeDataContainer to be used for
specifying input parameters operations like Simulation Import and Export. |
CaePart |
importSimulation(String solverName,
CaeDataContainer propertyList)
|
MaterialUtilities |
materialUtils()
|
Manager |
qualityAuditManager()
Returns the
Manager belonging to this session. |
void |
setFileNewContext(NXObject contextPart)
Sets the context part for use in naming new FEM, Sim, and Idealized parts in managed mode.
|
MaterialUtilities materialUtils() throws RemoteException
RemoteException
AssociationUtilities associationUtils() throws RemoteException
RemoteException
Manager qualityAuditManager() throws RemoteException
RemoteException
CaeDataContainer getDataContainer() throws NXException, RemoteException
CaeDataContainer
to be used for
specifying input parameters operations like Simulation Import and Export.
NXException
RemoteException
CaePart importSimulation(String solverName, CaeDataContainer propertyList) throws NXException, RemoteException
SimPart
and a FemPart
from
solver specific data. Import is driven by that properties defined in the input
CaeDataContainer
propertyList. The exact properties can vary from
solver to solver.
solverName
- the solver name to indicate what type of data is being importedpropertyList
- the import parameters see getDataContainer()
.NXException
RemoteException
void setFileNewContext(NXObject contextPart) throws NXException, RemoteException
contextPart
- the context partNXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.