Package | Description |
---|---|
nxopen.cae.connections |
Provides classes and interfaces relating to Connections.
|
Modifier and Type | Field and Description |
---|---|
static ConnectionDBItemStiffnessType |
ConnectionDBItemStiffnessType.CYLINDRICAL
Cylindrical
|
static ConnectionDBItemStiffnessType |
ConnectionDBItemStiffnessType.NONE
None
|
static ConnectionDBItemStiffnessType |
ConnectionDBItemStiffnessType.RECTANGULAR
Rectangular
|
static ConnectionDBItemStiffnessType |
ConnectionDBItemStiffnessType.SPHERICAL
Spherical
|
Modifier and Type | Method and Description |
---|---|
ConnectionDBItemStiffnessType |
ConnectionDBItemData.stiffnessType()
Returns the mass
License requirements: None. |
static ConnectionDBItemStiffnessType |
ConnectionDBItemStiffnessType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ConnectionDBItemStiffnessType |
ConnectionDBItemStiffnessType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ConnectionDBItemStiffnessType[] |
ConnectionDBItemStiffnessType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ConnectionDBItemData.setStiffnessType(ConnectionDBItemStiffnessType stiffnessType)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.