See: Description
Interface | Description |
---|---|
Adhesive |
Adhesive connection.
|
Bolt |
Bolt connection.
|
Bushing |
Bushing connection.
|
ComponentData |
Composer connection.
|
Composer |
Composer.
|
ComposerData |
Composer connection.
|
ConnectionData |
Composer connection.
|
ConnectionDBData |
Connection DB data.
|
ConnectionDBItemData |
Connection DB item data.
|
CoordinatesLocation |
Location interface.
|
CoordinatesSeriesLocation |
Location interface.
|
CurveLocation |
Location interface.
|
Damper |
Damper connection.
|
Element |
This is the class to access a connection element
To obtain an instance of this object use the Create creator in ElementCollection . |
ElementCollection |
Element collection provides methods to manage
Element objects
To obtain an instance of this class, refer to BaseFEModel Created in NX11.0.0 |
FeEdgesLocation |
Location interface.
|
Folder |
The Folder class offers a way to create a hierarchy of connections and sub-folders
To obtain an instance of this object use the add_folder creator in a parent folder or access connection root folder from IFEModel Created in NX12.0.0 |
IConnection |
This class represents an interface to a connection object.
|
ICsys |
This class represents an Interface to the Connection Csys.
|
IDiameter |
This class represents an Interface to the Diameter parameters.
|
IDof |
This class represents an interface to the connection's degrees of freedom.
|
IDofCombination |
This class represents an interface to the connection's degrees of freedom combination.
|
IFlangesContainer |
This interface offers access to the flanges of a connection (SpotWeld for example).
|
IHeight |
This class represents an Interface to the Height parameters.
|
ILineDiscretization |
This class represents an Interface to the Diameter parameters.
|
ILineOffset |
This class represents an Interface to the Diameter parameters.
|
ILocationsContainer |
This class represents an Interface to the Locations parameters.
|
ILocationsMultiPointContainer |
This class represents an Interface to the Multi Point Locations container.
|
ILocationsSinglePointContainer |
This class represents an Interface to the Locations parameters.
|
ILocationsWithDirContainer |
This class represents an Interface to the Locations parameters.
|
ILocationsWithDiscretizationContainer |
This class represents an Interface to the Locations With Discretization container.
|
IMaterial |
This class represents an Interface to the Material entity.
|
INodalTargetCenter |
This class represents an Interface to the Connection Target.
|
INodalTargetLegs |
This class represents an Interface to the Connection Target.
|
INodalTargetsContainer |
This class represents an Interface to the Connection Target Container.
|
INodalTargetsPairing |
This class represents an Interface to the nodal connections pairing algorithm parameters.
|
IStiffness |
This class represents an Interface to the Stiffness constants.
|
IStiffnessDynamic |
This class represents an Interface to the Stiffness dynamic.
|
IStructuralDamping |
This class represents an Interface to the StructuralDamping constants.
|
IStructuralDampingDynamic |
This class represents an Interface to the StructuralDamping dynamic.
|
ITolerance |
This class represents an Interface to the Tolerance parameters.
|
IViscousDamping |
This class represents an Interface to the ViscousDamping constants.
|
IViscousDampingDynamic |
This class represents an Interface to the ViscousDamping dynamic.
|
IWidth |
This class represents an Interface to the Width parameters.
|
Kinematic |
Kinematic connection.
|
Location |
Location base class.
|
LocationWithDir |
Location With Direction interface.
|
NodalTarget |
This class represents an Interface to the Connection Target.
|
NodalTargetSetOfPoints |
Set of Points Target.
|
NodalTargetSinglePoint |
Group of Points Target.
|
NodalTargetSpider |
Group of Points Target.
|
NodeLocation |
Location interface.
|
NodeSeriesLocation |
Location interface.
|
PointLocation |
Location interface.
|
PointSeriesLocation |
Location interface.
|
Rigid |
Rigid connection.
|
Sealing |
Sealing connection.
|
SeamWeld |
Seam Weld connection.
|
SelectionRecipeLocation |
Location interface.
|
SpotWeld |
Spot Weld connection.
|
Spring |
Spring connection.
|
Utils |
Contains universal connections utility methods
To obtain an instance of this class, refer to Folder Created in NX12.0.0 |
Class | Description |
---|---|
ComposerConnectionType |
composer Connection type
|
ConnectionDBItemStiffnessType |
connection DB item stiffness type
|
ConnectionType |
Connection type
|
CsysType |
Csys types
|
DiameterType |
Diameter definition types
|
Dof |
Degrees of freedom definition
|
DofCombination |
Degrees Of Freedom Combination types
|
DofType |
Degrees Of Freedom types
|
ElementStatusType |
Element status
|
ElementType |
Element type
|
HeadDiameterType |
Head diameter definition types
|
HeightType |
Types of height definitions
|
LocationDirectionType |
Location and Direction type
|
LocationType |
Location type
|
MaterialType |
Material definition types
|
ModelizationPPTRefTargetType |
Modelization PPTRefTargetType
|
ModelizationResultType |
Modelization result type
|
NodalPairingMethod |
Nodal pairing method
|
NodalTargetType |
Nodal Target types
|
SeamWeldMaterialType |
Seam Weld Material type
|
SeamWeldType |
Seam Weld Type
|
TargetDependencyType |
Nodal target dependency type
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.