Package | Description |
---|---|
nxopen.cae.connections |
Provides classes and interfaces relating to Connections.
|
Modifier and Type | Field and Description |
---|---|
static DofCombination |
DofCombination.CARDAN
DOF1 fixed, DOF2 fixed, DOF3 fixed, DOF4 free, DOF5 fixed, DOF6 free
|
static DofCombination |
DofCombination.CLAMP
DOF1 fixed, DOF2 fixed, DOF3 fixed, DOF4 fixed, DOF5 fixed, DOF6 fixed
|
static DofCombination |
DofCombination.PIVOT
DOF1 fixed, DOF2 fixed, DOF3 fixed, DOF4 free, DOF5 fixed, DOF6 fixed
|
static DofCombination |
DofCombination.POINT
DOF1 fixed, DOF2 free, DOF3 free, DOF4 free, DOF5 free, DOF6 free
|
static DofCombination |
DofCombination.SLIDER
DOF1 free, DOF2 fixed, DOF3 fixed, DOF4 fixed, DOF5 fixed, DOF6 fixed
|
static DofCombination |
DofCombination.SLIDER_PIVOT
DOF1 free, DOF2 fixed, DOF3 fixed, DOF4 free, DOF5 fixed, DOF6 fixed
|
static DofCombination |
DofCombination.SPHERIC
DOF1 fixed, DOF2 fixed, DOF3 fixed, DOF4 free, DOF5 free, DOF6 free
|
static DofCombination |
DofCombination.USER_DEFINED
User defined combination for all DOFs
|
Modifier and Type | Method and Description |
---|---|
DofCombination |
IDofCombination.dofCombination()
Returns the degrees of freedom combination type
License requirements: None. |
static DofCombination |
DofCombination.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DofCombination |
DofCombination.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DofCombination[] |
DofCombination.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
IDofCombination.setDofCombination(DofCombination type)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.