Package | Description |
---|---|
nxopen.cae.connections |
Provides classes and interfaces relating to Connections.
|
Modifier and Type | Field and Description |
---|---|
static HeadDiameterType |
HeadDiameterType.FACTOR_OF_DIAMETER
User defined relationship with bolt diameter
|
static HeadDiameterType |
HeadDiameterType.USER
User defined diameter
|
Modifier and Type | Method and Description |
---|---|
HeadDiameterType |
Bolt.headDiameterType()
Returns the head diameter type
License requirements: None. |
static HeadDiameterType |
HeadDiameterType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HeadDiameterType |
HeadDiameterType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HeadDiameterType[] |
HeadDiameterType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
Bolt.setHeadDiameterType(HeadDiameterType param)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.