public class HeadDiameterType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FACTOR_OF_DIAMETER
User defined relationship with bolt diameter
|
static int |
_USER
User defined diameter
|
static HeadDiameterType |
FACTOR_OF_DIAMETER
User defined relationship with bolt diameter
|
static HeadDiameterType |
USER
User defined diameter
|
Modifier and Type | Method and Description |
---|---|
static HeadDiameterType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HeadDiameterType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HeadDiameterType[] |
values()
Returns an array that contains the values for this enum.
|
public static final HeadDiameterType USER
public static final HeadDiameterType FACTOR_OF_DIAMETER
public static final int _USER
public static final int _FACTOR_OF_DIAMETER
public static HeadDiameterType valueOf(int value)
public static HeadDiameterType valueOf(String name)
public static HeadDiameterType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.