Package | Description |
---|---|
nxopen.cae.connections |
Provides classes and interfaces relating to Connections.
|
Modifier and Type | Field and Description |
---|---|
static DiameterType |
DiameterType.FORMULA
Formula defined diameter
|
static DiameterType |
DiameterType.TABLE_FILE
Table defined diameter
|
static DiameterType |
DiameterType.USER
User defined diameter
|
Modifier and Type | Method and Description |
---|---|
DiameterType |
IDiameter.diameterType()
Returns the diameter type
License requirements: None. |
DiameterType[] |
IDiameter.getSupportedDiameterTypes()
Gets supported diameter types of connection.
|
static DiameterType |
DiameterType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DiameterType |
DiameterType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DiameterType[] |
DiameterType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
IDiameter.setDiameterType(DiameterType diameterType)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.