Package | Description |
---|---|
nxopen.cae.connections |
Provides classes and interfaces relating to Connections.
|
Modifier and Type | Field and Description |
---|---|
static ComposerConnectionType |
ComposerConnectionType.BOLT
Bolt
|
static ComposerConnectionType |
ComposerConnectionType.BUMP_STOP
BumpStop
|
static ComposerConnectionType |
ComposerConnectionType.BUSHING
Bushing
|
static ComposerConnectionType |
ComposerConnectionType.KINEMATIC
Kinematic
|
static ComposerConnectionType |
ComposerConnectionType.LATCH
Latch
|
static ComposerConnectionType |
ComposerConnectionType.SEAM_WELD
SeamWeld
|
static ComposerConnectionType |
ComposerConnectionType.SPRING
Spring
|
static ComposerConnectionType |
ComposerConnectionType.WEATHER_STRIP
WeatherStrip
|
Modifier and Type | Method and Description |
---|---|
ComposerConnectionType |
ConnectionData.connectionType()
Returns the connection type
License requirements: None. |
static ComposerConnectionType |
ComposerConnectionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ComposerConnectionType |
ComposerConnectionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ComposerConnectionType[] |
ComposerConnectionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ConnectionData.setConnectionType(ComposerConnectionType type)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.