Package | Description |
---|---|
nxopen.cae.connections |
Provides classes and interfaces relating to Connections.
|
Modifier and Type | Field and Description |
---|---|
static LocationDirectionType |
LocationDirectionType.POINT
Two Points/Nodes
|
static LocationDirectionType |
LocationDirectionType.VECTOR
Points/Node and Vector
|
Modifier and Type | Method and Description |
---|---|
LocationDirectionType |
LocationWithDir.directionType()
Returns the direction type
License requirements: nx_masterfem ("Finite Element Modeling") . |
static LocationDirectionType |
LocationDirectionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LocationDirectionType |
LocationDirectionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LocationDirectionType[] |
LocationDirectionType.values()
Returns an array that contains the values for this enum.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.