public class LocationDirectionType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_POINT
Two Points/Nodes
|
static int |
_VECTOR
Points/Node and Vector
|
static LocationDirectionType |
POINT
Two Points/Nodes
|
static LocationDirectionType |
VECTOR
Points/Node and Vector
|
Modifier and Type | Method and Description |
---|---|
static LocationDirectionType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LocationDirectionType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LocationDirectionType[] |
values()
Returns an array that contains the values for this enum.
|
public static final LocationDirectionType POINT
public static final LocationDirectionType VECTOR
public static final int _POINT
public static final int _VECTOR
public static LocationDirectionType valueOf(int value)
public static LocationDirectionType valueOf(String name)
public static LocationDirectionType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.