Package | Description |
---|---|
nxopen.cae.connections |
Provides classes and interfaces relating to Connections.
|
Modifier and Type | Field and Description |
---|---|
static HeightType |
HeightType.DISTANCE_BETWEEN_FLANGES
Distance between flanges
|
static HeightType |
HeightType.DISTANCE_BETWEEN_FLANGES_MAX_OF_FLANGES_THICKNESS
Distance between flanges - Max of flanges thickness
|
static HeightType |
HeightType.DISTANCE_BETWEEN_FLANGES_MEAN_OF_FLANGES_THICKNESS
Distance between flanges - Mean of flanges thickness
|
static HeightType |
HeightType.MEAN_OF_FLANGES_THICKNESS
Mean of flanges thickness
|
static HeightType |
HeightType.UNDEFINED
Undefined height type, used for connections that don't use this parameter
|
static HeightType |
HeightType.USER
User defined thickness
|
Modifier and Type | Method and Description |
---|---|
HeightType[] |
IHeight.getSupportedHeightTypes()
Gets supported height types of connection.
|
HeightType |
IHeight.heightType()
Returns the height type
License requirements: None. |
static HeightType |
HeightType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HeightType |
HeightType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HeightType[] |
HeightType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
IHeight.setHeightType(HeightType heightType)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.