public class HeightType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DISTANCE_BETWEEN_FLANGES
Distance between flanges
|
static int |
_DISTANCE_BETWEEN_FLANGES_MAX_OF_FLANGES_THICKNESS
Distance between flanges - Max of flanges thickness
|
static int |
_DISTANCE_BETWEEN_FLANGES_MEAN_OF_FLANGES_THICKNESS
Distance between flanges - Mean of flanges thickness
|
static int |
_MEAN_OF_FLANGES_THICKNESS
Mean of flanges thickness
|
static int |
_UNDEFINED
Undefined height type, used for connections that don't use this parameter
|
static int |
_USER
User defined thickness
|
static HeightType |
DISTANCE_BETWEEN_FLANGES
Distance between flanges
|
static HeightType |
DISTANCE_BETWEEN_FLANGES_MAX_OF_FLANGES_THICKNESS
Distance between flanges - Max of flanges thickness
|
static HeightType |
DISTANCE_BETWEEN_FLANGES_MEAN_OF_FLANGES_THICKNESS
Distance between flanges - Mean of flanges thickness
|
static HeightType |
MEAN_OF_FLANGES_THICKNESS
Mean of flanges thickness
|
static HeightType |
UNDEFINED
Undefined height type, used for connections that don't use this parameter
|
static HeightType |
USER
User defined thickness
|
Modifier and Type | Method and Description |
---|---|
static HeightType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HeightType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HeightType[] |
values()
Returns an array that contains the values for this enum.
|
public static final HeightType UNDEFINED
public static final HeightType USER
public static final HeightType MEAN_OF_FLANGES_THICKNESS
public static final HeightType DISTANCE_BETWEEN_FLANGES
public static final HeightType DISTANCE_BETWEEN_FLANGES_MEAN_OF_FLANGES_THICKNESS
public static final HeightType DISTANCE_BETWEEN_FLANGES_MAX_OF_FLANGES_THICKNESS
public static final int _UNDEFINED
public static final int _USER
public static final int _MEAN_OF_FLANGES_THICKNESS
public static final int _DISTANCE_BETWEEN_FLANGES
public static final int _DISTANCE_BETWEEN_FLANGES_MEAN_OF_FLANGES_THICKNESS
public static final int _DISTANCE_BETWEEN_FLANGES_MAX_OF_FLANGES_THICKNESS
public static HeightType valueOf(int value)
public static HeightType valueOf(String name)
public static HeightType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.