Package | Description |
---|---|
nxopen.cae.connections |
Provides classes and interfaces relating to Connections.
|
Modifier and Type | Field and Description |
---|---|
static SeamWeldMaterialType |
SeamWeldMaterialType.ANGLE
Seam weld angle material type
|
static SeamWeldMaterialType |
SeamWeldMaterialType.DOUBLE
Seam weld double material type
|
static SeamWeldMaterialType |
SeamWeldMaterialType.OVERLAP
Seam weld overlap material type
|
Modifier and Type | Method and Description |
---|---|
static SeamWeldMaterialType |
SeamWeldMaterialType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SeamWeldMaterialType |
SeamWeldMaterialType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SeamWeldMaterialType[] |
SeamWeldMaterialType.values()
Returns an array that contains the values for this enum.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.