public class SeamWeldMaterialType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ANGLE
Seam weld angle material type
|
static int |
_DOUBLE
Seam weld double material type
|
static int |
_OVERLAP
Seam weld overlap material type
|
static SeamWeldMaterialType |
ANGLE
Seam weld angle material type
|
static SeamWeldMaterialType |
DOUBLE
Seam weld double material type
|
static SeamWeldMaterialType |
OVERLAP
Seam weld overlap material type
|
Modifier and Type | Method and Description |
---|---|
static SeamWeldMaterialType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SeamWeldMaterialType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SeamWeldMaterialType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SeamWeldMaterialType ANGLE
public static final SeamWeldMaterialType OVERLAP
public static final SeamWeldMaterialType DOUBLE
public static final int _ANGLE
public static final int _OVERLAP
public static final int _DOUBLE
public static SeamWeldMaterialType valueOf(int value)
public static SeamWeldMaterialType valueOf(String name)
public static SeamWeldMaterialType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.